15.2.6 Programming Production

The following figure shows the Microchip programming production flow. The flow supports simple programming jobs and bit stream file exports directly from the Libero tool, represented with the blue components in the following figure. Libero-based production flow only supports non-secured programming, based on KLK key mode. For more information, see the Libero SoC Design Flow User Guide .

The Job Manager extends that capability: allowing bit stream file and programming job generation outside of the Libero tool, and the support of SPPS flow, represented with green components in the following figure.

Figure 15-41. Microchip Programming Flow

Bitstream files (STAPL, DAT, and SPI) are programmed using FlashPro, DirectC, or Silicon Sculptor. STAPL file can be used by third party JTAG production programming tools to program Microchip devices. Programming jobs are supported by FlashPro Express only. The following figure shows the debug flow. It allows DDC generation outside of the Libero tool supports SPPS flow, represented with green components.

Figure 15-42. Microchip Debug Flow

The main SPPS flow is based on the use of HSM in the Operation and Production site. It supports the advanced production the programming models and SmartDebug as described in the following sections.