3.6.1 SmartHLS Pragmas Manual

Learn more about the pragmas available for SmartHLS.

3.6.1.1 Introduction to Pragmas

SmartHLS™ accepts pragma directives in the source code to guide the hardware generation. This reference section explains all of the pragmas available for SmartHLS.

The pragmas follow the following syntax:
#pragma HLS <category> <feature> <parameter>(<value>)
The category refers to the general usage class of the pragma. Each pragma has one of the following categories:
  • function: configure a hardware function.
  • loop: configure loop optimizations.
  • interface: configure hardware interfaces (arguments / global variables).
  • memory: configure hardware memory implementation.

Each category can have different configurable features. Some categories / features have parameters to passed to the pragma. A parameter can be optional with a default behaviour if not specified. The value of a parameter can be either integer, boolean (true|false), name (variable / argument), or a set of pre-specified values.

Note

Important:

For integer parameters, the user is allowed to use integer literals or integral constant expressions, which includes variables with constexpr specifiers, template parameters and macros defined using #define directive. For example, this is allowed:

#define N 10
void fun() {
  #pragma HLS loop unroll factor(N+1)
  for (int i = 0; i < 100; i++)
    ...
}
The pragma position is not arbitrary and placing the pragma in an incorrect position will cause an error. Each pragma can have one of the following positions:
  • At the beginning of function definition block before any other statements.
  • Before global / local variable declaration.
  • Before loop block.

3.6.1.2 Pipeline Loop

Syntax
#pragma HLS loop pipeline II(<int>)
Description
This pragma enables pipelining for a given loop in the code. Loop pipelining allows a new iteration of the loop to begin before the current one has completed, achieving higher throughput. It can be specified to pipeline a single loop or a nested loop. If specified on a single loop or on a inner loop of a nested loop, that loop will be pipelined. If specified on the outer loop of a nested loop, the outer loop will be pipelined and all of its inner loops will be automatically unrolled.
Parameters
ParameterValueOptionalDefaultDescription
IIIntegerYes1Pipeline initiation interval
Position
Before the beginning of the loop. If there is a loop label, the pragma should be placed after the label.
Examples
#pragma HLS loop pipeline II(2)
for (int i = 0; i < 10; i++) {
  ...
}
LOOP_LABEL:
#pragma HLS loop pipeline
while (i < 10) {
  ...
}

3.6.1.3 Unroll Loop

Syntax
#pragma HLS loop unroll factor(<int>)
Description
Specifies a loop to be unrolled. The factor indicates how many times to unroll the loop. If it is not specified, or specified as N (the total number of loop iterations), the loop will be fully unrolled. If it is specified as 2, the loop will be unrolled 2 times, where the number of loop iterations will be halved and the loop body will be replicated twice. If it is specified as 1, the loop will NOT be unrolled.
Parameters
ParameterValueOptionalDefaultDescription
factorIntegerYesN (fully unroll)Unroll count
Position
Before the beginning of the loop. If there is a loop label, the pragma should be placed after the label.
Examples
#pragma HLS loop unroll factor(1)
for (int i = 0; i < 10; i++) {
  ...
}

3.6.1.4 Bound Loop

Syntax
#pragma HLS loop bounds lower(<int>) upper(<int>)
Description
Specifies the bounds on the number of times a loop will iterate. This pragma does not affect the synthesized circuit. It's only used to improve reporting. By manually specifying bounds, the overall loop latency can be computed and reported.
Parameters
ParameterValueOptionalDefaultDescription
lowerIntegerNo-Lower bound
upperIntegerNo-Upper bound
Position
Before the beginning of the loop. If there is a loop label, the pragma should be placed after the label.
Examples
#pragma HLS loop bounds lower(5) upper(10)
// Here, the bounds tell us the trip count (number of iterations) will be between 5 and 10 inclusively.
for (int i = 0; i < N; i++) {
  ...
}

3.6.1.5 Loop Dependence

Syntax
#pragma HLS loop dependence variable(<var_name>) type(inter) direction(RAW|WAR|WAW) dependent(true|false)
#pragma HLS loop dependence argument(<arg_name>) type(inter) direction(RAW|WAR|WAW) dependent(true|false)
Description
Specifies the loop-carried dependence of a variable to eliminate false dependency and improve pipeline initiation interval (II). HLS loop dependence pragma configuration overrides the loop dependency analysis result in the tool.
Important: Users are advised to carefully verify the loop dependency information specified. An incorrect loop dependency information leads the tool to generate incorrect hardware design.
Parameters
ParameterValueOptionalDefaultDescription
variable/argumentStringNo-Variable/Argument Name.
typeinterNo-Dependence Type. inter is the dependence between different loop iterations.
directionRAW|WAR|WAWYes-Specifies the loop dependence direction. Only valid for type(inter). When direction is not specified, the dependent parameter is applicable to all 3 directions.
dependenttrue|falseNo-Specifies if there is a loop-carried dependence for the given type and direction.
Position
Before the beginning of the loop. If there is a loop label, the pragma should be placed after the label.
Examples
int f(int x[100], int j /*j is odd*/) {
  int res = 0;
loop:
  #pragma HLS loop pipeline
  #pragma HLS loop dependence argument(x) type(inter) direction(RAW) dependent(false)
  for (int i = 0; i < 100; i = i + 2 /*i is even*/) {
     res += x[i];
     x[i + j] += 1;
  }
  return res;
}

3.6.1.6 Inline Function

Syntax
#pragma HLS function inline
Description
This pragma forces a given function to be inlined.
Position
At the beginning of the function definition block.
Examples
int sum(int *a) {
#pragma HLS function inline
  ...
}

3.6.1.7 Noinline Function

Syntax
#pragma HLS function noinline
Description
This pragma prevents a given function from being inlined.
Position
At the beginning of the function definition block.
Examples
int sum(int *a) {
#pragma HLS function noinline
  ...
}

3.6.1.8 Replicate Function

Syntax
#pragma HLS function replicate
Description
This pragma specifies a function to be replicated every time it is called. By default, when the circuit is not pipelined, SmartHLS™ creates a single instance for each function which is shared across multiple calls to the function. When using this pragma on the function, SmartHLS will create a new instance of the function for every function call.
Position
At the beginning of the function definition block.
Examples
int sum(int *a) {
#pragma HLS function replicate
  ...
}

3.6.1.9 Flatten Function

Syntax
#pragma HLS function flatten branchless(true|false)
Description
This pragma unrolls all loops and inlines all subfunctions for a given function. If the branchless option is set to true, all branches (e.g., if-else, switch) in the specified function will also be flattened to allow more parallelism between operations, specifically between the operations that are under different-yet-independent conditions.
Parameters
ParameterValueOptionalDefaultDescription
branchlesstrue|falseYestruetrue to flatten branch statements
Position
At the beginning of the function definition block.
Examples
int sum(int *a) {
#pragma HLS function flatten branchless(true)
  ...
}

3.6.1.10 Set Top-Level Function

Syntax
#pragma HLS function top
Description
This pragma specifies the top-level C/C++ function. The top-level function and all of its descendant functions will be compiled to hardware. SmartHLS currently does not support nesting top-level functions. The top-level function can only be called from a software testbench.
Position
At the beginning of the function definition block.
Examples
int sum(int *a) {
#pragma HLS function top
  ...
}

3.6.1.11 Pipeline Function

Syntax
#pragma HLS function pipeline II(<int>)
Description
This pragma enables pipelining for a given function in the code. Function pipelining allows a new invocation of a function to begin before the current one has completed, achieving higher throughput.
Parameters
ParameterValueOptionalDefaultDescription
IIIntegerYes1Pipeline initiation interval
Position
At the beginning of the function definition block.
Examples
int sum(int *a) {
#pragma HLS function pipeline
  ...
}
int conv(int a[], int b[]) {
#pragma HLS function pipeline II(3)
  ...
}

3.6.1.12 Dataflow

Syntax
#pragma HLS function dataflow
Description
Specifies that a function should execute using dataflow parallelism.
Position
At the beginning of the function definition block.
Examples
void canny(hls::FIFO<unsigned char> &input_fifo,
           hls::FIFO<unsigned char> &output_fifo) {
#pragma HLS function dataflow

#pragma HLS dataflow_channel variable(output_gf) type(fifo)
    unsigned char output_gf [HEIGHT * WIDTH];
#pragma HLS dataflow_channel variable(output_sf) type(fifo)
    unsigned short output_sf [HEIGHT * WIDTH];
#pragma HLS dataflow_channel variable(output_nm) type(fifo)
    unsigned char output_nm [HEIGHT * WIDTH];

    gaussian_filter(input_fifo, output_gf);
    sobel_filter(output_gf, output_sf);
    nonmaximum_suppression(output_sf, output_nm);
    hysteresis_filter(output_nm, output_fifo);
}

3.6.1.13 Dataflow Channel

Syntax
#pragma HLS dataflow_channel variable(<var_name>) type(fifo|shared_buffer|double_buffer) depth(<int>)
Description
Specifies that a variable in a dataflow function should be converted to use a particular channel type.
Parameters
ParameterValueOptionalDefaultDescription
variablestringNo-Variable Name
typefifo|shared_buffer|double_bufferNo-Channel type
depthIntegerYes2FIFO depth (only when type is FIFO)
Position
Before the variable declaration.
Examples
FIFO channels are used for a Canny edge detector, since the pixels are processed in sequential order.
void canny(hls::FIFO<unsigned char> &input_fifo,
           hls::FIFO<unsigned char> &output_fifo) {
#pragma HLS function dataflow

#pragma HLS dataflow_channel variable(output_gf) type(fifo)
    unsigned char output_gf [HEIGHT * WIDTH];
#pragma HLS dataflow_channel variable(output_sf) type(fifo)
    unsigned short output_sf [HEIGHT * WIDTH];
#pragma HLS dataflow_channel variable(output_nm) type(fifo)
    unsigned char output_nm [HEIGHT * WIDTH];

    gaussian_filter(input_fifo, output_gf);
    sobel_filter(output_gf, output_sf);
    nonmaximum_suppression(output_sf, output_nm);
    hysteresis_filter(output_nm, output_fifo);
}

3.6.1.14 Scalar Argument Interface

Syntax
#pragma HLS interface argument(<arg_name>) type(<simple|axi_target>) stable(<false|true>)
Description
This pragma configures the RTL interface for a scalar argument. This pragma is ignored if the enclosing function is not specified as the top-level.
Parameters
ParameterValueOptionalDefaultDescription
argumentstringNoArgument name
typesimple|axi_targetNosimpleInterface type
stabletrue|falseYesfalseOnly available for simple type; true if the argument is stable.
Position
At the beginning of the function definition block.
Examples
int fun(int a) {
#pragma HLS function top
#pragma HLS interface argument(a) type(simple) stable(true)
  ...
}

3.6.1.15 Memory Interface for Pointer Argument/Global Variable

Syntax
#pragma HLS interface argument(<arg_name>) type(memory) num_elements(<int>)

#pragma HLS interface variable(<var_name>) type(memory) num_elements(<int>)

Description
This pragma specifies the memory interface type for a pointer (including array, struct, class types) argument or shared global variable. For more details, see the Memory Interface section. This pragma is ignored if the enclosing function is not specified as the top-level.
Parameters
ParameterValueOptionalDefaultDescription
argument/variablestringNo-Argument/Variable name
typememoryNo-Interface type
num_elementsintegerYes-Specifies the number of elements of the argument array. Can override the array size in the argument.
Position

Argument - At the beginning of the function definition block.

Variable - Before the global variable declaration.

Examples
#pragma HLS interface variable(c) type(memory) num_elements(100)
int c[100];

int fun(int a[], int b[]) {
#pragma HLS function top
#pragma HLS interface argument(a) type(memory) num_elements(100)
#pragma HLS interface argument(b) type(memory)
  ...
}

3.6.1.16 AXI4 Target Interface for Pointer Argument

Syntax
#pragma HLS interface argument(<arg_name>) type(axi_target) num_elements(<int>) dma(true|false) requires_copy_in(true|false)
Description
This pragma specifies the AXI4 target interface type for a pointer (including array, struct, class types) argument. For more details, see the AXI4 Target Interface section. This pragma is ignored if the enclosing function is not specified as the top-level.
Parameters
ParameterValueOptionalDefaultDescription
argumentstringNo-Argument name
typeaxi_targetNo-Interface type
num_elementsintegerYes-Specifies the number of elements of the argument array. Can override the array size in the argument.
dma, requires_copy_intrue|falseYesfalseSpecifies the transfer method and copy-in behaviour in the top-level driver function. See Top-level Driver Options in Pointer Arguments' AXI4 Target Interface Pragma
ecctrue|falseYesfalseSpecifies if Error Correction Code is enabled. Set to true for enabling ECC for AXI4 Target Interface. See Error Correction Code for more information about Error Correction Code.
Position
At the beginning of the function definition block.
Examples
int fun(int a[], int b[101]) {
#pragma HLS function top
#pragma HLS interface argument(a) type(axi_target) num_elements(100) dma(true) requires_copy_in(false)
#pragma HLS interface argument(b) type(axi_target)
  ...
}

3.6.1.17 AXI4 Initiator Interface for Pointer Argument

Syntax
#pragma HLS interface argument(<arg_name>) type(axi_initiator) ptr_addr_interface(<simple|axi_target>) num_elements(<int>) max_burst_len(<int>) max_outstanding_reads(<int>) max_outstanding_writes(<int>)
Description
This pragma specifies the AXI4 initiator interface type for a pointer (including array, struct, class types) argument. For more details, see the AXI4 Initiator Interface section. This pragma is ignored if the enclosing function is not specified as the top-level.
Parameters
ParameterValueOptionalDefaultDescription
argumentstringNo-Argument name
typeaxi_initiatorNo-Interface type
num_elementsintegerYes-Specifies the number of elements of the argument array. Can override the array size in the argument. Only needed by the Simulate HLS Hardware (SW/HW Co-Simulation) feature and does not affect HLS-generated RTL.
ptr_addr_interfacesimple|axi_targetYes-Specifies the interface type for setting the base address of the accessing memory. The default type is simple but is changed to axi_target if Default All Interfaces to Use AXI4 Target is set.
max_burst_lenintegerYes16Specifies the maximum burst length for each AXI initiator transaction. Transfers that are larger than the maximum burst length will be split into multiple AXI transactions. The permitted values are between 1 and 256.
max_outstanding_readsintegerYes1Specifies the maximum amount of read burst requests to external AXI4 Targets that can be left outstanding (waiting for response) before the accelerator stalls. This infers a FIFO of size max_outstanding_reads*addr_size for the AR channel, and a FIFO of size max_outstanding_reads*max_burst_len*word_size for the R channel. The permitted values are between 1 and 8.
max_outstanding_writesintegerYes1Specifies the maximum amount of write burst requests to external AXI4 Targets that can be left outstanding (waiting for response) before the accelerator stalls. This infers a FIFO of size max_outstanding_writes*addr_size for the AW channel, and a FIFO of size max_outstanding_writes*max_burst_len*word_size for the W channel. The permitted values are between 1 and 8.
add_4k_boundary_protectionboolYestrueSpecifies whether or not SmartHLS™ should generate additional logic to protect AXI4 initiator burst transactions from crossing 4K boundaries for this argument. Setting this field to false will remove this alignment logic, but the user must then make sure that any pointer addresses given to the SmartHLS module will not result in bursting accross a 4K address boundary (a violation of the AXI4 spec.
Position
At the beginning of the function definition block.
Examples
int fun(int a[]) {
#pragma HLS function top
#pragma HLS interface argument(a) type(axi_initiator) num_elements(100) ptr_addr_interface(axi_target) max_burst_len(8)
#pragma HLS interface argument(a) type(axi_initiator) num_elements(100) max_outstanding_reads(4) max_outstanding_writes(4)
  ...
}

3.6.1.18 Legacy AXI4 Slave Interface for Global Variable

Syntax
#pragma HLS interface variable(<var_name>) type(axi_slave) concurrent_access(true|false)
Description
This pragma specifies the legacy AXI4 slave interface for a global struct. When the concurrent_access option is set to true (default to false), the external logic can read/write the AXI4 slave interface while the SmartHLS module is running. The concurrent access will however reduce the SmartHLS module's throughput to access the memory. For more details. see the Legacy AXI4 Slave Interface section. This pragma is ignored if the enclosing function is not specified as the top-level.
Parameters
ParameterValueOptionalDefaultDescription
variablestringNo-Variable name
typeaxi_slaveNo-Interface type
concurent_accesstrue|falseYesfalseEnable/disable concurrent access
Position
Before the global variable declaration.
Examples
#pragma HLS interface variable(b) type(axi_slave) concurrent_access(true)
int b[SIZE];

3.6.1.19 Module Control Interface

Syntax
#pragma HLS interface control type(<simple|axi_target>)
Description
This pragma configures the Module Control Interface. This pragma is ignored if the enclosing function is not specified as the top-level.
Parameters
Table 3-18. 
ParameterValueOptionalDefaultDescription
typesimple|axi_targetNosimpleInterface type
Position
At the beginning of the function definition block.
Examples
int fun() {
#pragma HLS function top
#pragma HLS interface control type(simple)    ...
}

3.6.1.20 Default All Interfaces to Use AXI4 Target

Syntax
#pragma HLS interface default type(axi_target)
Description
This pragma specifies the default interface to AXI4 target for all arguments and Module Control Interface. This pragma is ignored if the enclosing function is not specified as the top-level.
Parameters
ParameterValueOptionalDefaultDescription
typeaxi_target No-Interface type
Position
At the beginning of the function definition block.
Examples
// The following two functions have the same interface configurations.

// Without using default interface pragma:
int fun(int a, int b[10], int c[20], int d[30]) {
#pragma HLS function top
#pragma HLS interface control     type(axi_target)
#pragma HLS interface argument(a) type(axi_target)
#pragma HLS interface argument(b) type(axi_target)
#pragma HLS interface argument(c) type(axi_target) dma(true)
#pragma HLS interface argument(d) type(axi_initiator) ptr_addr_interface(axi_target)
  ...
}

// Use default interface pragma:
int fun(int a, int b[10], int c[20], int d[30]) {
#pragma HLS function top
#pragma HLS interface default     type(axi_target)
#pragma HLS interface argument(c) type(axi_target) dma(true)
// Note that 'ptr_addr_interface(axi_target)' can be omitted when default interface is set to axi_target.  #pragma HLS interface argument(d) type(axi_initiator)
  ...
}

3.6.1.21 Contention-Free Memory Access

Syntax
#pragma HLS memory impl variable(<arg_name>) contention_free(true|false)
Description
The pragma is to be used for variables accessed by parallel functions (hls::thread) so that SmartHLS™ does not create arbiters for the specified variable. The specified variable can still be accessed by multiple concurrently running functions, but without contention. It will be the users' responsibility to ensure at most one function may access the shared variable in a clock cycle. If not specified, by default, SmartHLS creates arbiters for variables that are accessed by parallel functions.
Parameters
ParameterValueOptionalDefaultDescription
variablestringNo-Variable Name
contention_freetrue|falseNo-true for contention-free access
Position
Before the global / local variable declaration.
Examples
#pragma HLS memory impl variable(b) contention_free(true)
int b[100]

3.6.1.22 Struct Variable/Argument Packing

Syntax
#pragma HLS memory impl variable(<var_name>) pack(bit|byte) byte_enable(true|false)

#pragma HLS memory impl argument(<arg_name>) pack(bit|byte) byte_enable(true|false)

Description
The pragma is to be used to pack a global interface / local memory variable with struct type. There are two packing modes: bit/ byte where bit packing packs the struct fields using the exact bit-width and byte mode packs the fields with 8-bit alignment. byte_enable option creates an interface / memory with byte enable signals to write individual fields when set to true. Note that byte_enable is only valid with byte packing.
Parameters
ParameterValueOptionalDefaultDescription
variable/argumentstringNo-Variable/Argument Name
packbit|byteNo-Packing Mode
byte_enabletrue|falseYesfalseUse byte-enable to write stuct fields
Position

Argument - At the beginning of the function definition block.

Variable - Before the global / local variable declaration.

Examples
#pragma HLS memory impl variable(b) pack(bit)
struct S b[100];

int sum(struct S &s) {
#pragma HLS function top
#pragma HLS memory impl argument(s) pack(byte) byte_enable(true)
 ...
}

3.6.1.23 Partition Memory

Syntax
#pragma HLS memory partition variable(<var_name>) type(block|cyclic|complete|struct_fields|none) dim(<int>) factor(<int>)
Description
This pragma specifies a variable to be partitioned. Dimension 1 corresponds to the left-most dimension of an array and higher dimensions correspond to right-ward dimensions. The dim parameter is only applicable for block|cyclic|complete types. If dim is 0, the specified partitioning will be applied to all dimensions. The factor parameter is only applicable for block|cyclic types to specify the number of partitions. factor must be larger than 1. For more details about the pragma options, see User-Specified Memory Partitioning.
Parameters
ParameterValueOptionalDefaultDescription
variablestringNo-Variable name
typeblock, cyclic, complete, struct_fields, noneYescompletePartition type
dimintegerYes0Partition dimension
factorintegerYes-Number of partitions
Position
Before the global / local variable declaration.
Examples
#pragma HLS memory partition variable(b) type(none)
int b[100];

int fun(int *a) {
  ...
  #pragma HLS memory partition variable(c) type(block) dim(1) factor(2)
  int c[100][100];
  ...
}

3.6.1.24 Partition Top-Level Interface

Syntax
#pragma HLS memory partition argument(<arg_name>) type(block|cyclic|complete|struct_fields|none) dim(<int>) factor(<int>)
Description
This pragma specifies a top-level argument to be partitioned. Dimension 1 corresponds to the left-most dimension of an array and higher dimensions correspond to right-ward dimensions. The dim parameter is only applicable for block|cyclic|complete types. If dim is 0, the specified partitioning will be applied to all dimensions. The factor parameter is only applicable for block|cyclic types to specify the number of partitions. factor must be larger than 1. For more details about the pragma options, see .User-Specified Memory Partitioning
Parameters
ParameterValueOptionalDefaultDescription
argumentstringNo-Argument name
typeblock, cyclic, complete, struct_fields, noneYescompletePartition type
dimintegerYes0Partition dimension
factorintegerYes-Number of partitions
Position
At the beginning of the function definition block.
Examples
int sum(int *a, int *b) {
#pragma HLS function top
#pragma HLS memory partition argument(a) type(cyclic) dim(2) factor(4)
#pragma HLS memory partition argument(b)
}

3.6.1.25 Replicate ROM

Syntax
#pragma HLS memory replicate_rom variable(<rom_var_name>) max_replicas(<int>)
Description
This pragma can be used to replicate constant memory (i.e., arrays) to achieve better throughput (shorter cycle latency) at the expense of extra resource (e.g., block RAM). Typically when an array is implemented in block RAMs, there are up-to-two RAM ports to allow a maximum of two reads per clock cycle. To allow more parallel read accesses in each clock cycle, constant read-only memories (ROM) can be replicated by using this pragma.
The optional max_replicas can be used to control the maximum number of replicas. If a max_replicas of N is specified, SmartHLS™ will make sure to use no more than N replicas of the ROM in the generated circuit; the generated circuit may use less than N replicas when the throughput cannot be further improved with more replicas. When max_replicas is unspecified or set to 0, the number of replicas is unlimited and SmartHLS will use as many replicas as it needs to maximize throughput. A max_replicas of 1 means only one copy is allowed, hence no replication, equivalent to not having the pragma.
Parameters
ParameterValueOptionalDefaultDescription
variablestringNo-Variable name
max_replicasintegerYes0The maximum number of replicas allowed
Position
Before the global / local variable declaration.
Examples
#pragma HLS memory replicate_rom variable(my_rom) max_replicas(10)
const int my_rom[100]

3.6.1.26 Error Correction Code

Syntax
#pragma HLS memory impl variable(<var_name>) ecc(true|false)
Description
This pragma enables generating Error Correction Code (ECC) protected memory.
Parameters
ParameterValueOptionalDefaultDescription
variablestringNo-Variable name
ecctrue|falseNo-true for enabling ECC
Position
Before the global / local variable declaration.
Examples
#pragma HLS memory impl variable(x) ecc(true)
int x[100];