21.12.12 remove_non_actel_device_from_database

Description

This Tcl command removes settings for non-Microchip or non-Actel device from the device database.

remove_non_actel_device_from_database [-name {device name}]

Arguments

ParameterTypeDescription
namestringSpecifies the non-Actel or non-Microchip device name to be removed from the database. You can repeat this argument for multiple devices.
Return TypeDescription
NoneNone

Error Codes

Error CodeDescription
NoneRequired parameter 'name' is missing.
NoneThe device 'device_name' does not exist in the database.
NoneParameter 'name' is missing or has invalid value.
NoneParameter 'name' has illegal value.
NoneParameter 'param_name' is not defined. Valid command formatting is 'remove_non_actel_device_from_database [-name "name"]+'.

Supported Families

Supported Families
PolarFire®
PolarFire SoC
RTG4™
SmartFusion® 2
IGLOO® 2

Example

The following example removes the "F1502AS" device from the database:

remove_non_actel_device_from_database -name {F1502AS}

See Also

  • add_non_actel_device_to_database