Programming Overview
This document defines the programming specification for the dsPIC33AK512MC510 and dsPIC33AK512MPS512 Digital Signal Controller (DSC) devices:
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
The programming is implemented via the In-Circuit Serial Programming™ (ICSP™) interface, which includes the clock and data pins (PGECx and PGEDx).
The dsPIC33AK512MC510 and dsPIC33AK512MPS512 devices have a
Nonvolatile Memory (NVM) controller module. This NVM module performs the device Flash
memory programming. Its operation is configured and managed by the CPU. The external
programmer tool uses the serial programming interface (ICSP) to shift in and execute CPU
instructions, move data in and out of the device, and configure the NVM controller for
programming operations. The programmer sends MOV instructions to the
CPU to store (prepare) the Flash data to be programmed in the device RAM, or NVM control
registers, depending on the Programming mode. Then, the programmer executes CPU
instructions to initiate an erase or write operation using the NVM controller. To read
Flash data from the device, a VISI register is implemented. The content of this register
can be shifted out to the ICSP interface. For fast Flash content verification, the NVM
controller supports a CRC-32 checksum engine. It can reduce the amount of data which
should be read over the ICSP communications pins. Figure explains the interactions between the programmer and device.