1 Flash Memory
The Flash memory on dsPIC33AK512MC510 and dsPIC33AK512MPS512 family devices is divided into quadwords (16 bytes each), write rows (512 bytes each) and erase pages (4096 bytes each). The quadword (four 32-bit long words) is the minimum data size which can be written into the Flash. The address of each quadword is aligned by 16 bytes. Also, the Flash memory can be written by rows. Each row consists of 32 quadwords or 512 bytes. The address of each row is aligned by 512-byte boundaries.
The Flash must be erased before a write operation can be initiated. The Flash can be erased by pages. Each erase page consists of eight rows or 4096 bytes. The address of each erase page is aligned by 4096-byte boundaries.
The dsPIC33AK512MC510 and dsPIC33AK512MPS512 family devices’ Flash memory regions are shown in Table 1-1.
| Memory Region | Address | Number of Quadwords | Number of Write Rows | Number of Erase Pages | ||
|---|---|---|---|---|---|---|
| User OTP | 0x7F2C00-0x7F2FFC | 64 | 2 | Not applicable | ||
| User Configuration A1 (UCA1) | 0x7F3000-0x7F3FFC | 256 | 8 | 1 | ||
| User Configuration B (UCB) | 0x7F4000-0x7F4FFC | 256 | 8 | 1 | ||
| User Configuration A2 (UCA2) | 0x7FB000-0x7FBFFC | 256 | 8 | 1 | ||
| Code Memory | 256-Kbyte Flash Memory Devices | Single Boot | 800000-83FFFC | 16,384 | 512 | 64 |
| Dual Boot | 800000-81FFFC | 8,182 | 256 | 32 | ||
| C00000-C1FFFC | 8,182 | 256 | 32 | |||
| 512-Kbyte Flash Memory Devices | Single Boot | 800000-87FFFC | 32,768 | 1024 | 128 | |
| Dual Boot | 800000-83FFFC | 16,384 | 512 | 64 | ||
| C00000-C3FFFC | 16,384 | 512 | 64 | |||
Some dsPIC33AK512MC510 and dsPIC33AK512MPS512 family device registers are used in the programming procedures. These registers’ addresses and descriptions are listed in Table 1-2.
| Register Name | Address | Description |
|---|---|---|
| VISI | 0x0007C0 | This register moves (shifts) data out of the device through the ICSP™ interface. |
| NVMCON | 0x003000 | This register selects type and initiates an erase or write Flash operation. |
| NVMADR | 0x003004 | The destination Flash address for erase or write operations. |
| NVMDATA0 | 0x003008 | This register with data is programmed to Flash when quadword write is used. |
| NVMDATA1 | 0x00300C | This register with data is programmed to Flash when quadword write is used. |
| NVMDATA2 | 0x003010 | This register with data is programmed to Flash when quadword write is used. |
| NVMDATA3 | 0x003014 | This register with data is programmed to Flash when quadword write is used. |
| NVMSRCADR | 0x003018 | This register should be set to the address of the RAM buffer loaded with the Flash row data to be programmed. |
| NVMCRCCON | 0x003048 | This register controls the Cyclic Redundancy Check (CRC) calculation of the Flash region. |
| NVMCRCST | 0x00304C | This register contains the start address of the 4-Kbyte Flash memory block for the CRC calculation. |
| NVMCRCEND | 0x003050 | This register contains the end address of the 4-Kbyte Flash memory block minus one byte for the CRC calculation. |
| NVMCRCSEED | 0x003054 | The initial CRC value (seed) should be loaded into this register. If the CRC-32 is calculated for the multiple memory blocks, then the previous CRC result must be written directly to NVMCRCSEED before the next block of CRC calculations. |
| NVMCRCDATA | 0x003058 | This register contains the CRC calculation result. |