1.1.2.2 SAME70 Xplained Ultra

The following picture shows the SAME70 Xplained Ultra board connected with PL460-EK and REB215-XPRO expansion boards:

Figure 1-8. SAME70 Xplained Ultra + PL460-EK + REB215-XPRO

PL460-EK is connected to EXT1 connector (J602) of SAME70 Xplained Ultra. Since the enclosure of PL460-EK does not fit with SAME70 Xplained Ultra, the user must be very careful if the PLC wire is connected to the mains because not all the board is isolated from mains (PLC signal). For more information about PL460-EK refer to its user guide.

REB215-XPRO is connected to EXT2 connector (J604) of SAME70 Xplained Ultra. For more information about REB215-XPRO refer to its user guide.

REB215-XPRO is only used in the PLC-RF Hybrid projects (see Table 1-1). In the PLC-RF Hybrid projects, it is possible to connect only one expansion board and the application runs correctly, with only PLC or RF PHY Sniffer Tool available.

The Debug USB connector (J300) of SAME70 Xplained Ultra can be used to:
  • Flash/debug the SAME70 device with the on-board Microchip Embedded Debugger (EDBG)
The Target USB connector (J200) of SAME70 Xplained Ultra can be used to:
  • Send/receive USI messages to/from Microchip Hybrid Sniffer PC Tool
In order to use the Target USB, the J203 jumper must be connected between VBUS and PB08.

For more information about SAME70 Xplained Ultra refer to its user guide.