1.2.2.1.3 Library Interface
This section describes the Application Programming Interface (API) functions of the Networking Presentation Layer.
| Name | Description |
|---|---|
| System Functions | |
| NET_PRES_Deinitialize | Deinitializes the Network Presentation Layer Instance. |
| NET_PRES_Initialize | Initializes the Network Presentation Layer sub-system with the configuration data. |
| NET_PRES_Reinitialize | Reinitializes the instance of the presentation layer. |
| NET_PRES_Tasks | MPLAB Harmony tasks function used for general presentation layer tasks. |
| NET_PRES_Status | Provides the current status of the MPLAB Harmony Networking Presentation Layer. |
| Socket Functions | |
| NET_PRES_SocketBind | Binds a socket to a local address. |
| NET_PRES_SocketClose | Disconnects an open socket and destroys the socket handle, releasing the associated resources. |
| NET_PRES_SocketConnect | Connects a client socket. |
| NET_PRES_SocketDiscard | Discards any pending data in the RX FIFO. |
| NET_PRES_SocketDisconnect | Disconnects an open socket. |
| NET_PRES_SocketEncryptSocket | This function turns an insecure socket into a secure socket. Details: This function will turn an unencrypted socket into an encrypted socket and starts encryption negotiation. |
| NET_PRES_SocketFlush | Immediately transmits all pending TX data. |
| NET_PRES_SocketGetTransportHandle | This function returns the transport layer handle. Details: This function returns the transport layer handle for a valid socket |
| NET_PRES_SocketInfoGet | Obtains information about a currently open socket. |
| NET_PRES_SocketIsConnected | Determines whether a socket has an established connection. |
| NET_PRES_SocketIsNegotiatingEncryption | This function checks if encryption negotiation is still in progress. |
| NET_PRES_SocketIsOpenModeSupported | Checks to see if a mode is supported by open. |
| NET_PRES_SocketIsSecure | This function checks whether a connection is secure. |
| NET_PRES_SocketLastError | This function returns the last error code for this socket. Details: This function will return the last error code that was set for this socket and it will clear the current error code. An error code is set whenever a socket operation fails for some missing functionality, bad parameter, etc. |
| NET_PRES_SocketOpen | Opens a presentation socket. |
| NET_PRES_SocketOptionsGet | Allows the options for a socket such as, current RX/TX buffer size, etc., to be obtained. |
| NET_PRES_SocketOptionsSet | Allows setting options to a socket like adjust RX/TX buffer size, etc. |
| NET_PRES_SocketPeek | Reads a specified number of data bytes from the RX buffer/FIFO without removing them from the buffer. |
| NET_PRES_SocketRead | Reads an array of data bytes from a socket's RX buffer/FIFO. |
| NET_PRES_SocketReadIsReady | Determines how many bytes can be read from the RX buffer. |
| NET_PRES_SocketRemoteBind | Binds a socket to a remote local address. |
| NET_PRES_SocketSignalHandlerDeregister | Deregisters a previously registered socket signal handler. |
| NET_PRES_SocketSignalHandlerRegister | Registers a socket signal handler. |
| NET_PRES_SocketWasReset | Self-clearing semaphore indicating socket reset. |
| NET_PRES_SocketWrite | Takes a buffer and sends it to the encryption provider. |
| NET_PRES_SocketWriteIsReady | Determines how much free space is available in the TX buffer. |
| Certificate Store Functions | |
| NET_PRES_CertStoreGetCACerts | This function gets the CA certificates from the store, |
| NET_PRES_CertStoreGetServerCert | This function gets a server certificate and key from the certificate store. |
| Data Types and Constants | |
| _NET_PRES_EncProviderObject | Defines the data that the presentation layer needs from the provider. |
| _NET_PRES_TransportObject | Defines the data that the transport layer needs to provide to the Networking Presentation Layer. |
| NET_PRES_INDEX | Sets the type for the presentation layer index. |
| NET_PRES_INIT_DATA | Initializes a Presentation layer. |
| NET_PRES_INST_DATA | Initializes a Presentation layer. |
| NET_PRES_SIGNAL_FUNCTION | MPLAB Harmony Networking Presentation Layer Signal function. |
| NET_PRES_SIGNAL_HANDLE | Sets the type for the presentation layer signal handle. |
| NET_PRES_SKT_HANDLE_T | Sets the type for the presentation layer socket handle. |
| NET_PRES_ADDRESS | NET_PRES address |
| NET_PRES_EncProviderConnect | Connects the function to the provider. |
| NET_PRES_EncProviderConnectionClose | Defines the close function to the provider. |
| NET_PRES_EncProviderDeinit | Defines the deinitialization function for the provider. |
| NET_PRES_EncProviderInit | Defines the initialization function to the encryption provider. |
| NET_PRES_EncProviderIsInitialized | Determines whether the encryption provider has been initialized. |
| NET_PRES_EncProviderObject | Defines the data that the presentation layer needs from the provider. |
| NET_PRES_EncProviderOpen | Defines the open connection function to the provider. |
| NET_PRES_EncProviderRead | Defines the read function to the provider |
| NET_PRES_EncProviderWrite | Defines the write function to the provider. |
| NET_PRES_EncSessionStatus | Defines the enumeration for the state and status of the encrypted portion of a connection. |
| NET_PRES_SKT_ADDR_T | NET_PRES address type |
| NET_PRES_SKT_ERROR_T | NET_PRES error type |
| NET_PRES_SKT_OPTION_TYPE | NET_PRES option type |
| NET_PRES_SKT_PORT_T | Sets the type for the presentation layer port. |
| NET_PRES_SKT_T | NET_PRES socket type |
| NET_PRES_TRANS_ADDR_T | Defines a generic address structure to pass to the transport layer. |
| NET_PRES_TRANS_ADDRESS_TYPE | Defines the enumeration for the type of address. |
| NET_PRES_TRANS_OPTION_T | Defines the enumeration for the type of options. |
| NET_PRES_TransBind | Binds a socket to a local address. |
| NET_PRES_TransBool | Generic function prototype for functions that return a bool. |
| NET_PRES_TransClose | Function prototype for functions that closes a socket. |
| NET_PRES_TransDiscard | Function prototype for functions that clears a socket's RX buffer. |
| NET_PRES_TransHandlerRegister | Function prototype that registers a handler with a socket. |
| NET_PRES_TransOpen | Opens a presentation socket. |
| NET_PRES_TransOption | Sets of gets a socket's options. |
| NET_PRES_TransPeek | Function prototype for functions that peeks on the socket's buffer. |
| NET_PRES_TransportObject | Defines the data that the transport layer needs to provide to the Networking Presentation Layer. |
| NET_PRES_TransRead | Defines the read function provided by the transport layer. |
| NET_PRES_TransReady | Defines the ready function provided by the transport layer. |
| NET_PRES_TransSignalHandlerDeregister | Function prototype that deregisters a handler with a socket. |
| NET_PRES_TransSocketInfoGet | Function prototype for functions that gets the information on a socket. |
| NET_PRES_TransWrite | Defines the write function provided by the transport layer. |
| NET_PRES_INVALID_SOCKET | Invalid socket indicator macro. |
| NET_PRES_CERTSTORE_H | This is macro NET_PRES_CERTSTORE_H. |
| NET_PRES_ENCRYPTION_PROVIDER_API_H | This is macro NET_PRES_ENCRYPTION_PROVIDER_API_H. |
| NET_PRES_SOCKET_API | This is macro NET_PRES_SOCKET_API. |
| NET_PRES_TRANSPORT_API_H | This is macro NET_PRES_TRANSPORT_API_H. |
| NET_PRES_H | This is macro NET_PRES_H. |
| NET_PRES_EncProviderReadReady | Defines the read ready function to the provider |
| NET_PRES_EncProviderWriteReady | Defines the write ready function to the provider. |
| NET_PRES_TransIsPortDefaultSecured | Checks to see if a port is encrypted by default. |
| NET_PRES_EncProviderMaxOutputSize | Defines the maximum output size function to the provider. |
| NET_PRES_EncProviderOutputSize | Defines the output size function to the provider. |