1.2.4.4.2 Internet Management Protocol (IGMP) Configurations
IGMP Specific User Configurations
Number of IGMP Interfaces:
The maximum number of interfaces that support IGMP
Should be <= interfaces that are present at the stack initialization
Default value: 1
Symbol TCPIP_IGMP_INTERFACES
Number of Multicast Groups:
Maximum number of multicast groups (addresses) for which a IGMP application can subscribe
Each group can listen to multiple sources
Should be prime number for best performance
Default value: 7
Symbol TCPIP_IGMP_MCAST_GROUPS
Number of Sources in Each Group:
Maximum number of multicast sources per group a IGMP application can listen to
Each multicast source can be used by multiple sockets
Should be prime number for best performance
Note: the 'all sources' (TCPIP_IGMP_ASM_ALL_SOURCES) may take a slot!
Note: Should be <= 32
Note: if TCPIP_IGMPV2_SUPPORT_ONLY is enabled then this value is ignored
Default value: 11
Symbol TCPIP_IGMP_SOURCES_PER_GROUP
Number of Socket Records per Source:
Maximum number of socket records that are part of a IGMP source multicast address for a specific group G
Note that same socket may need multiple records if it listens on multiple interfaces!
When operating in IGMPv2 style, it represents the total number of sockets that can join/leave a specific group.
Default value: 4
Symbol TCPIP_IGMP_SOCKET_RECORDS_PER_SOURCE
IGMP Task Rate (in msec):
IGMP task processing rate, in milliseconds.
The IGMP module will process a timer event with this rate for maintaining its own queues, processing timeouts, etc.
The lower the rate (higher the frequency) the higher the module priority and higher module performance can be obtained
The value cannot be lower than the TCPIP_STACK_TICK_RATE.
Default value: 33
Symbol TCPIP_IGMP_TASK_TICK_RATE
Default Robustness Variable Value:
The default Robustness Variable value
The Robustness Variable allows tuning for the expected packet loss on a network.
If a network is expected to be lossy, the Robustness Variable may be increased.
IGMP is robust to (Robustness Variable - 1) packet losses.
RFC 3376 IGMPv3: The Robustness Variable MUST NOT be zero, and SHOULD NOT be one. Default: 2
This is just a default value. The actual value is taken from a router query.
Default value: 2
Symbol TCPIP_IGMP_ROBUSTNESS_VARIABLE
Default Unsolicited Report Interval (in msec):
The default Unsolicited Report Interval
The Unsolicited Report Interval is the time between repetitions of a host�s initial report of membership in a group.
RFC 3376 IGMPv3: Default: 1 second.
Value is in milliseconds
Default value: 1000
Symbol TCPIP_IGMP_UNSOLICITED_REPORT_INTERVAL
IGMPv2 Support Only:
If this symbol is !0, then only Join and Leave operations are supported, without support for source addresses required by IGMPv3
This results in smaller code and less RAM needed by the IGMP module.
Default value: false
Symbol TCPIP_IGMPV2_SUPPORT_ONLY
Enable User Notification Functions:
Enable/disable user notification functions
Default value: false
Symbol TCPIP_IGMP_USER_NOTIFICATION