1.2.4.7.2 Neighbor Discovery Protocol (NDP) Configurations
NDP Specific User Configurations
NDP Task Rate (in msec):
NDP task processing rate, in milliseconds.
The NDP module will process a timer event with this rate for maintaining its own queues, processing timeouts, etc.
The lower the rate (higher the frequency) the higher the module priority and higher module performance can be obtained
The value cannot be lower than the TCPIP_STACK_TICK_RATE.
Value is in milliseconds
Default value: 32
Symbol TCPIP_NDP_TASK_TIMER_RATE, TCPIP_IPV6_NDP_TASK_TIMER_RATE
RTR Solicitation Delay (in sec):
Router Solicitation Delay
Value is in seconds
Default value: 1
Symbol TCPIP_MAX_RTR_SOLICITATION_DELAY, TCPIP_IPV6_NDP_MAX_RTR_SOLICITATION_DELAY
RTR Solicitation Interval (in sec):
Router Solicitation Interval
Value is in seconds
Default value: 4
Symbol TCPIP_RTR_SOLICITATION_INTERVAL, TCPIP_IPV6_NDP_RTR_SOLICITATION_INTERVAL
Maximum RTR Solicitations:
Maximum number of router solicitations
Default value: 3
Symbol TCPIP_MAX_RTR_SOLICITATIONS, TCPIP_IPV6_NDP_MAX_RTR_SOLICITATIONS
Maximum Multicast Solicitations:
Maximum number of multicast solicitations
Default value: 3
Symbol TCPIP_MAX_MULTICAST_SOLICIT, TCPIP_IPV6_NDP_MAX_MULTICAST_SOLICIT
Maximum Unicast Solicitations:
Maximum number of unicast solicitations
Default value: 3
Symbol TCPIP_MAX_UNICAST_SOLICIT, TCPIP_IPV6_NDP_MAX_UNICAST_SOLICIT
Maximum Anycast Delay Time (in sec):
Maximum anycast delay time
Value is in seconds
Default value: 1
Symbol TCPIP_MAX_ANYCAST_DELAY_TIME, TCPIP_IPV6_NDP_MAX_ANYCAST_DELAY_TIME
Maximum Neighbor Advertisement Transmissions:
Maximum number of neighbor advertisement transmissions
Default value: 3
Symbol TCPIP_MAX_NEIGHBOR_ADVERTISEMENT, TCPIP_IPV6_NDP_MAX_NEIGHBOR_ADVERTISEMENT
Reachable Time (in sec):
Value for the reachable time
Value is in seconds
Default value: 30
Symbol TCPIP_REACHABLE_TIME, TCPIP_IPV6_NDP_REACHABLE_TIME
Re-transmission Timer (in sec):
Value of the retransmission timer
Value is in seconds
Default value: 1
Symbol TCPIP_RETRANS_TIMER, TCPIP_IPV6_NDP_RETRANS_TIMER
Delay First Probe Time (in sec):
Value of the delay for the first probe
Value is in seconds
Default value: 5
Symbol TCPIP_DELAY_FIRST_PROBE_TIME, TCPIP_IPV6_NDP_DELAY_FIRST_PROBE_TIME
IPv6 MTU Increase Time-out (in sec):
Sets the maximum transmit unit increase timeout
Value is in seconds
Default value: 600
Symbol TCPIP_IPV6_MTU_INCREASE_TIMEOUT