TCPIP_ICMP_CallbackDeregister Function
C
bool TCPIP_ICMP_CallbackDeregister(
ICMP_HANDLE hIcmp
);
Description
This function notifies a stack client to remove its former registered notification handler. After this operation the client will no longer be notified about the receiving of replies to the ICMP requests.
Preconditions
The TCP/IP Stack must be initialized and up and running. A previous successful call to TCPIP_ICMP_CallbackRegister has been done.
Parameters
Parameters | Description |
---|---|
hIcmp | An ICMP handle obtained by TCPIP_ICMP_CallbackRegister. |
Returns
True - If the notification handler has bee successfully removed.
False - If such a notification handler could not be found.
Remarks
None.
Example
void MyICMPCallbackFunction(TCPIP_NET_HANDLE hNetIf, IPV4_ADDR * remoteIP, void * data);
ICMP_HANDLE hIcmp = TCPIP_ICMP_CallbackRegister(&MyICMPCallbackFunction);
if(hIcmp != 0)
{
// successfully registered my handler
// send requests and process the incoming results
// ...
// later on, once we're done, remove the notification handler
TCPIP_ICMP_CallbackDeregister(hIcmp);
}