6.2 Example Output
The output format of the example project can be seen in the following figure. This example is with the setting SAMPLE_PERIOD set to 2 (seconds).
The output format of the example project can be seen in the following figure. This example is with the setting SAMPLE_PERIOD set to 2 (seconds).