1.3.1 The PWM's Tri-State Setting of the Auto-Shutdown Feature Will Not Drive the Pin to Tri-State
The tri-state setting of the auto-shutdown feature in the enhanced PWM will not successfully drive the pin to tri-state. The pin will remain an output and should not be driven externally. All tri-state settings will be affected.
Work around
Use one of the other two auto-shutdown states available as outlined in the data sheet.
Affected Silicon Revisions
| A2 | A3 | A4 | A6 | A7 | |||
| X | X | X | X | X |