1.5.1 Entering Ultra Low-Power Sleep Mode By Setting
RETEN = 0 and SRETEN
= 1Will Cause the Device to Become Unprogrammable Through ICSP™
Entering Ultra Low-Power Sleep mode by setting RETEN =
0 and SRETEN = 1 will
cause the device to not be programmable through ICSP™. This issue occurs when the
RETEN bit in CONFIG1L is cleared to '0',
the SRETEN bit in the WDTCON register is set to
'1' and a SLEEP instruction is executed within the
first 350 μs of code execution. This happens after a Reset event, causing the device to
enter Ultra Low-Power Sleep mode.
Work around
SLEEP instruction when ULP
is enabled. To ensure the Ultra Low-Power Sleep mode is not enabled, the
RETEN bit in CONFIG1L should be set to a
'1' and the SRETEN bit in the WDTCON
register should be cleared to a '0'. The following code can be
used:
// This will ensure the RETEN bit is set to '1' #pragma config RETEN = OFF // This will ensure that the SRETEN bit is '0' WDTCONbits.SRETEN = 0;
If the Ultra Low-Power Sleep mode is needed, the user must ensure that the minimum
time, before the first SLEEP instruction is executed, is greater
than 350 μs.
Affected Silicon Revisions
| A2 | A3 | A4 | A6 | A7 | |||
| X |