3.3.3 Getting Started Application Using Harmony v3 Drivers on PIC32CZ CA70 Curiosity Ultra Development Kit Using FreeRTOS
Description
The application reads the current room temperature from the temperature sensor on the I/O1 Xplained Pro Extension kit. The temperature reading is displayed on a serial console periodically every second. In addition, the application writes the temperature readings to EEPROM. When a character is entered on the console, the last five written temperature values are read from the EEPROM and displayed on the console. An LED (LED0) on the PIC32CZ CA70 Curiosity Ultra kit is toggled every time the temperature is displayed on the serial console.
Modules/Technology Used
- Peripheral Modules
- PIO
- UART
- TWIHS
- NVIC
- EFC
- Drivers
- USART
- I2C
- Third Party Libraries
- FreeRTOS - Kernel
Hardware Used
Software/Tools Used
This project has been verified to work with the following versions of software tools:
- MPLAB X IDE v6.25
- MPLAB Code Configurator Plugin v5.6.2
- MPLAB XC32 Compiler v4.60
- csp v3.22.0
- core v.3.15.1
- FreeRTOS - Kernal v11.2.0
- CMSIS_5 v5.9.0
- PIC32CZ-CA70_DFP v1.0.10
Refer to the Project Manifest present in harmony-manifest-success.yml
under the project folder
pic32cz_ca70_cult_getting_started_freertos/firmware/src/config/pic32cz_ca70_cult.
- Refer to the Release Notes to know the MPLAB X IDE and MCC Plug-in version
- Any Serial Terminal application, such as Tera Term terminal application
Due to Microchip regularly updates tools, occasionally issue(s) could be discovered while using the newer versions of the tools. If the project does not seem to work and version incompatibility is suspected. It is recommended to double-check and use the same versions that the project was tested with. To download original version of MPLAB Harmony v3 packages, refer to the document How to Use the MPLAB Harmony v3 Project Manifest Feature (DS90003305).
Setup
- Verify that the temperature sensor (I/O1 Xplained Pro Extension kit) is connected to Extension Header 1 (EXT1) on the PIC32CZ CA70 Curiosity Ultra development kit
- Connect the Type-A male to
Micro-B USB cable to Micro-B DEBUG USB port (J900) to program and debug the
PIC32CZ CA70 Curiosity Ultra development kit
Programming Hex File
The pre-built hex file can be programmed by following the below steps.
Steps to program the hex file- Open MPLAB X IDE
- Close all existing projects in IDE, if any project is opened
- Go to File>Import>Hex/ELF file
- In the Import Image File window,
- Create Prebuilt Project,
- Click the Browse button to select the prebuilt hex file
- Select Device as PIC32CZ2051CA70144
- Ensure the proper tool is selected under Hardware Tool and click the Next button
- Select Project Name and
Folder,
- Select appropriate project name and folder and click the Finish button
- Create Prebuilt Project,
- In MPLAB X IDE, click the Make and Program Device button to program the device
- Follow the steps in Running the Demo section below
Programming/Debugging Application Project
- Open the project
(
pic32cz_ca70_cult_getting_started_freertos/firmware/pic32cz_ca70_cult.X) in MPLAB X IDE - Ensure
PIC32CZ CA70 Curiosity Ultrais selected as hardware tool to program/debug the application - Build the code and program the device by clicking on the Make and Program button in MPLAB X IDE tool bar
- Follow the steps in Running the Demo section below
Running the Demo
- Open the Tera Term terminal application on the PC (from the Windows Start menu by pressing the Start button)
- Set the baud rate to 115200
- Reset or power cycle the device
- The user should see the
temperature values (in °F) being displayed on the terminal every 500
milliseconds, as shown below
- Notice the LED0 blinking at 1 second rate
- Press any character on the
terminal to display the last five values written to the EEPROM
- The user may vary the
temperature by placing the finger on the temperature sensor (for a few
seconds)
Comments
- Reference Training Module: MPLAB® Harmony v3 Drivers on SAM E70/S70/V70/V71 MCUs Using FreeRTOS™: Getting Started.
- This application demo builds
and works out of box by following the instructions above in Running the Demo
section. If the user needs to enhance/customize this application demo,
should use the MPLAB Harmony v3 Software framework. Refer to the following
links to setup and build the applications using MPLAB Harmony.
- How to Setup MPLAB Harmony v3 Software Development Framework (DS90003232)
- How to Build an Application by Adding a New PLIB, Driver, or Middleware to an Existing MPLAB Harmony v3 Project (DS90003253)
- Video - How to Set up the Tools Required to Get Started with MPLAB® Harmony v3 and MCC
- Create a new MPLAB Harmony v3 project using MCC
- Update and Configure an Existing MHC-based MPLAB Harmony v3 Project to MCC-based Project