44.4 OPA Operation with ADC
When INTOE
= 1, the OPA module provides internal
connections directly to the ADC, allowing it to be used for
analog signal conditioning before a signal is converted by the
ADC. In this mode of operation, the external output of the OPA
connected to the OPAxOUT pin is disabled, and the internal
output of the OPA module is available to be selected as an ADC
input through the ADC channel selection register. When using
this mode of operation, the ADPCH register of the ADC module
must be used to select one of the available OPA input pins. The
OPA input pin selection determined using the ADC input channel
selection register will take precedence over the input pin
selection using the PSS bits. The noninverting OPA input
will switch to the pin selected by the ADPCH, and the OPA output
will be connected to the ADC input.
1, the external output of the OPA
module is disabled and the OPAxOUT pin can be used
as a GPIO.