7 File System

The WINCS02 provides an internal secured storage for storing following types of certificates and keys to use with the Transport Layer Security (TLS).

  • x509 root certificates
  • Client/Device certificates
  • Private keys

The secured certificate store is of 60 KB in size and it is write and erase only storage space. The certificates and keys flashed in this memory is only readable through the device firmware.

The certificate store can be accessed through the API's.

The manual certificate/key flashing would need a serial terminal application with X-Modem/Y-Modem file transfer support. In order to simplify this process the firmware release package includes a python based utility which can Flash these files through a simple CLI

The utility also support Send To option on Windows operating system where these files can be flashed into WINCS02 device through the right click options.

By default the WINCS02 modules include following Root Certificates in the certificate store for easier could connectivity.
Table 7-1. Pre-packaged TLS Root Certificates
IssuerFilenameExpiryPublic KeySignature Alg.Notes
Amazon Root CA 1AmazonRootCA1.der17 January 2038 01:00:00RSA (2048 bits)SHA256RSAAWS Cloud
Baltimore CyberTrust RootBaltimoreCyberTrustRoot.der13 May 2025 00:59:00RSA (2048 bits)SHA1RSAAzure Cloud
DigiCert High Assurance EV Root CADigiCert.der10 November 2031 01:00:00RSA (2048 bits)SHA1RSA—
DigiCert Global Root G2DigiCertGlobalRootG2.crt15 January 2038 13:00:00RSA (2048 bits)SHA256RSAAzure Cloud
DigiCert High Assurance EV Root CADigiCertSHA2.der22 October 2028 13:00:00RSA (2048 bits)SHA256RSA—
Entrust Root Certification AuthorityEnTrust.der27 November 2026 21:53:42RSA (2048 bits)SHA1RSA—
GlobalSign Root CAGlobalSignRoot.der28 January 2028 13:00:00RSA (2048 bits)SHA1RSA—
Internet Security Research Group Root X1isrgrootx1.der04 June 2035 12:04:38RSA (4096 bits)SHA256RSALetsEncrypt
QuoVadis Root CA 2QuoVadis_Root.der24 November 2031 19:23:33RSA (4096 bits)SHA1RSA—
VeriSign Class 3 Primary Certification AuthorityVeriSign.der17 July 2036 00:59:59RSA (2048 bits)SHA1RSA—

Setup Details – The PC companion mode (simillar to RNWF02) of the setup must be used to use the certificate and key utility.

Note: To operate the WINCS02 Add On Board in PC Companion mode, ensure to place the jumper cap on J201.1, J201.2.

The simplest method to use the WINCS02 Add On Board is to connect it to a PC host that supports USB CDC virtual COM (serial) ports using the on-board MCP2200 USB-to-UART converter. The user can send ASCII commands to the WINCS02 Module using a terminal emulator application. In this case, the PC acts as the host device. In addition to UART, Wake and Interrupt pin from WINCS02 Module are also connected to MCP2200’s GPIO pins. This enables to set low power modes via Host PC. The MCP2200 is configured in Reset condition until the USB supply is plugged in.

Figure 7-1. AT Commands Terminal
Table 7-2. WINCS02 Connection to MCLR, INT0/WAKE, IRQ
Pin on MCP2200Pin on WINCS02 ModuleDescription
GP0NCNC
GP1NCNC
GP2MCLRWINCS02 Module Reset
GP3INT0/WAKEInput pin to WINCS02 Module to bring out from the Deep sleep/Extreme Deep sleep mode to the WAKE mode.
GP4IRQOutput pin from WINCS02 Module to indicate data activity.
GP5NCNC
GP6NCNC
GP7NCNC