8.6.6.2 Power Management
The programmer must first enable the CAN clock in the Power Management Controller (PMC) before using the CAN.
A Low-power mode is defined for the CAN controller. If the application does not require CAN operations, the CAN clock can be stopped when not needed and be restarted later. Before stopping the clock, the CAN controller must be in Low-power mode to complete the current transfer. After restarting the clock, the application must disable the Low-power mode of the CAN controller.