9.4.6.10.1 Input-Output Transfer Functions

The ADC can be configured to operate in the following input voltage modes:

  • Single-Ended—ADC_CCR.DIFFx = 0 and ADC_PDR.PDIFFx = 0. This is the default mode after a reset.
  • Differential—ADC_CCR.DIFFx = 1 and ADC_PDR.PDIFFx = 0 (see the figure below). In Differential mode, the ADC requires differential input signals having a VDD/2 common mode voltage (refer to the section “Electrical Characteristics”).
  • • Pseudo-Differential—ADC_PDR.PDIFFx = 1. In Pseudo-Differential mode, one of the analog pins is used as the negative input of the ADC (see table Input Pins and Channel Numbers in Pseudo-Differential Mode). The ADC samples the other analog inputs with respect to this one. The common mode input range is 0 to VDD (refer to the section “Electrical Characteristics”).

The following equations provide the unsigned ADC input-output transfer function in each mode(1). With signed conversions (see field ADC_EMR.SIGNMODE), subtract 2047 from the ADC_LCDR.DATA value given below. Note that the Single-Ended mode introduces a x2 gain compared to the Pseudo-Differential mode.

In the formula, REFP = VREFP, REFN = VREFN.

Single-Ended mode:

ADC_LCDR.LDATA=ADx−REFNREFP−REFN×212

Differential mode:

ADC_LCDR.LDATA=1+ADx−ADx+1REFP−REFN×211

Pseudo-Differential mode:

ADC_LCDR.LDATA=1+ADx−AD11REFP−REFN×211
Note: Equations assume ADC_EMR.OSR = 1

If ADC_MR.ANACH is set, the ADC can manage both differential channels and single-ended channels. If ADC_MR.ANACH is cleared, the parameters defined in ADC_CCR are applied to all channels.

The following tables provide the internal positive and negative ADC inputs assignment with respect to the programmed mode (ADC_CCR.DIFFx and ADC_PDR.PDIFFx).

For example, if Differential mode is required on channel 0, input pins AD0 and AD1 are used. In this case, only channel 0 must be enabled by writing a 1 to ADC_CHER.CH0.

Table 9-6. Input Pins and Channel Numbers in Single-Ended and Differential Modes
Internal ADC Inputs (VIN+, VIN-)Channel Number
Single-Ended ModeDifferential ModeSingle-Ended ModeDifferential Mode
AD0, ADVREFNAD0, AD1CH0CH0
AD1, ADVREFN–CH1
AD2, ADVREFNAD2, AD3CH2CH2
AD3, ADVREFN–CH3
AD4, ADVREFNAD4, AD5CH4CH4
AD5, ADVREFN–CH5
AD6, ADVREFNAD6, AD7CH6CH6
AD7, ADVREFN–CH7
AD8, ADVREFNAD8, AD9CH8CH8
AD9, ADVREFN–CH9
AD10, ADVREFNAD10, AD11CH10CH10
AD11, ADVREFN–CH11

In Pseudo-Differential mode, inputs are managed by a 12/2:1-channel analog multiplexer. See the table below.

Table 9-7.  Input Pins and Channel Numbers in Pseudo-Differential Mode
Internal ADC Inputs (VIN+, VIN-)Channel Number
AD0, AD11CH0
AD1, AD11CH1
AD2, AD11CH2
AD3, AD11CH3
AD4, AD11CH4
AD5, AD11CH5
AD6, AD11CH6
AD7, AD11CH7
AD8, AD11CH8
AD9, AD11CH9
AD10, AD11CH10
AD11, AD11CH11
Figure 9-31. Analog Full Scale Ranges in Single-Ended/Pseudo-Differential/Differential Applications