22.3.2.3.1 One Ramp Mode
In One Ramp mode, the TCD counter counts up until it reaches the CMPBCLR value. Then the TCD cycle is done and the counter restarts from 0x000, beginning a new TCD cycle. The TCD cycle period is:
In the figure above, CMPASET < CMPACLR < CMPBSET < CMPBCLR.
This is required in One Ramp mode to avoid overlapping outputs. The figure below is an
example where CMPBSET < CMPASET < CMPACLR < CMPBCLR, resulting in an
overlap of the outputs. If any of the other compare values are bigger than CMPBCLR it will never be
triggered when running in One Ramp mode, and if the CMPACLR is smaller than the CMPASET
value, the clear value will not have any effect.