3.1 Macro Configurations
Below are the macro configurations in the main.c file.
- Application with four use case
options, with defined values 1 to 4 respectively, as shown below:
#define FREE_RUNNING 1 #define SINGLE_CONVERSION 2 #define WINDOW_COMPARATOR_MODE 3 #define SAMPLE_ACCUMULATOR 4 - Which use case to run is selected
by changing the value of the macro
EXAMPLE_CODE:#define EXAMPLE_CODE SAMPLE_ACCUMULATOR - The following macros are also
used in case it can easily be changed afterward. Maximum input voltage:
#define MAX_VOL 2.5 //VREF=2.5VMaximum input reference voltage is configured to 2.5V to calculate the voltage for measured ADC reading.
Note: ADC reference (VREF) has been configured to 2.5V. - ADC result resolution:
#define RES_10BIT 0x3FFADC resolution has been configured to be 10 bits, with the maximum result value of 0x3FF.
- ADC input channel:
#define ADC_CHANNEL 5ADC input signal has been connected to channel 5: AIN5 (pin PA5).