5.8.1.4 External Functions

Functions that are defined outside the projects C source files (e.g., a function defined in a separate bootloader project or in an assembly module) will require declarations so that the compiler knows how to encode calls to those functions.

A function declaration will look similar to the following example. Note that the extern specifier is optional, but make it clear this is a declaration.

extern int clockMode(int);