9.2.2 di Macro
A macro that disables interrupts.
Include
<xc.h>
Prototype
void di(void);
Remarks
This macro clears the GIE bit in the INTCON register. The MCC-generated
INTERRUPT_GlobalInterruptDisable()
function performs the same task as the
di()
macro .
Example
See the notes at the beginning of this chapter or section for
information on using printf()
or scanf()
(and other functions reading and writing the stdin
or
stdout
streams) in the example code.
#include <xc.h>
#include <stdio.h>
unsigned int count;
void __interrupt() myIsr (void) {
if(INTCONbits.TMR0IE == 1 && INTCONbits.TMR0IF == 1) {
INTCONbits.TMR0IF = 0;
TMR0 = timer0ReloadVal;
count++;
}
}
unsigned int getTicks(void) {
unsigned int val;
di(); /* disable interrupts */
val = count; /* protected non-atomic operation */
ei(); /* re-enable interrupts */
return val;
}
int main(void) {
SYSTEM_Initialize(); /* MCC generated code */
INTERRUPT_GlobalInterruptEnable(); /* MCC alternative to ei() */
INTERRUPT_PeripheralInterruptEnable();
while(getTicks() < 0x400) /* wait for 0x400 overflows */
continue;
INTERRUPT_GlobalInterruptDisable(); /* MCC alternative to di() */
printf("done");
while(1)
continue;
}