5.14.2 Predefined Macros
The compiler drivers define certain symbols to the preprocessor, allowing conditional compilation based on chip type, etc. The symbols listed in the table below show the more common symbols defined by the drivers.
Each symbol, if defined, is equated to 1 (unless otherwise stated).
| Symbol | Set |
|---|---|
ERRATA_4000_BOUNDARY | When the ERRATA_4000 applies. |
MPLAB_ICD | When building for an MPLAB ICD debugger. Assigned 2 to 5 to indicate an MPLAB ICD 2 through MPLAB ICD 5, respectively. |
_CHIPNAME | When the specific chip type selected, e.g.,
_16F877. |
_BANKBITS_ | When building for non-PIC18 devices. Assigned 0, 1, or 2 to indicate 1, 2, or 4 available banks or RAM. |
_BANKCOUNT_ | When building for non-PIC18 devices. Indicates the number of banks of data memory implemented. |
_COMMON_ | When common RAM is present. |
_COMMON_ADDR_ | When common memory is present. Indicates common memory starting address. |
_COMMON_SIZE_ | When common memory is present. Indicates the common memory size. |
_EEPROMSIZE | When building for non-PIC18 devices. Indicates how many bytes of EEPROM are available. |
_EEPROM_INT | When building for non-PIC18 devices. Assigned
a value of 2 (_NVMREG_INT), 1 (_EEREG_INT),
or 0 (_NOREG_INT) to indicate the device uses the NVMREG,
EEREG, or no register interface to access EEPROM. |
_ERRATA_TYPES | When the errata workaround is being applied,
see -merrata option, Errata Option. |
_FAMILY_FAMILY_ | When building for PIC18 devices and indicates
the PIC18 family as indicated by the FAMILY field in the
relevant .ini file in the compiler's
pic/dat/ini directory. |
_FLASH_ERASE_SIZE | Always. Indicates the size of the Flash program memory erase block. They do not represent Flash data memory. |
_FLASH_WRITE_SIZE | Always. Indicates the size of the Flash program memory write block. They do not represent Flash data memory. |
_GPRBITS_ | When building for non-PIC18 devices. Assigned 0, 1, or 2 to indicate 1, 2, or 4 available banks or general purpose RAM. |
_GPRCOUNT_ | When building for non-PIC18 devices. Assigned a value which indicates the number of banks that contain general-purpose RAM. |
_HAS_FUNCTIONLEVELPROF_ | When -finstrument-functions
is specified and target supports profiling. |
_HAS_INT24 | Always. |
_HAS_OSCVAL_ | When the target device has an oscillator calibration register. |
_MPC_ | When compiling for Microchip PIC MCU family. |
_OMNI_CODE_ | When compiling using an OCG compiler. |
_PIC12 | When building for a Baseline device (12-bit instruction). |
_PIC12E | When building for an Enhanced Baseline device (12-bit instruction). |
_PIC12IE | When building for am Enhanced Baseline device with interrupts. |
_PIC14 | When building for an Mid-range device (14-bit instruction). |
_PIC14E | When building for an Enhanced Mid-range device (14-bit instruction). |
_PIC14EX | When building for an extended-bank Enhanced Mid-range PIC device (14-bit instruction). |
_PIC18 | When building for a PIC18 device (16-bit instruction). |
_PROGMEM_ | When building for a Mid-range device with flash memory, and indicates the type of flash memory employed by the target device: values 0xFF (unknown) 0xF0 (none) 0 (read-only) 1 (word write with auto erase) 2 (block write with auto erase) 3 (block write with manual erase). |
_PTR3_ADDR_MASK | Always set for PIC18 projects to a value that when ANDed with a 24-bit mixed-space address will mask any bits representing the target memory space, leaving just the target address offset. |
_RAMSIZE | When building for a PIC18 device. Indicates how many bytes of data memory are available. |
_ROMSIZE | Always. Indicates how much program memory is available (byte units for PIC18 devices; words for other devices). |
__CHIPNAME and
__CHIPNAME__ | When the specific chip type selected, e.g., __16F877. |
__CLANG__ | Always |
__CODECOV | When code coverage is enabled, with value
__CC_RAM (1). |
__DATABANK | When eeprom or flash memory is implemented, and identifies in which bank the EEDATA/PMDATA register is found. |
__DATE__ | Always. Indicates the current date as a
string literal, e.g., "May 21 2004". |
__DEBUG | When performing a debug build and you are using the MPLAB X IDE. |
__EXTMEM | When device has external memory. Indicates the size of this memory. |
__FILE__ | Always. Indicates the source file being preprocessed. |
__FLASHTYPE | When building for non-PIC18 devices with
flash memory. Indicates the type of flash memory employed by the target device,
see _PROGMEM below. |
__LINE__ | Always. Indicates this source line number. |
__J_PART | When building for a PIC18 ‘J’ series part. |
__MPLAB_ICDX__ | When compiling for an ICD debugger.
X can be 2,
3, 4, or 5 indicating a
Microchip MPLAB ICD 2, ICD 3, ICD 4, or ICD 5 respectively. |
__MPLAB_ICE__ | To indicate any In-circuit Emulator |
__MPLAB_ICE4__ | When compiling for a Microchip ICE 4 In-Circuit Emulator. |
__MPLAB_PICKITX__ | When compiling for a PICkit™.
X can be 2,
3, 4, or 5 indicating a
Microchip MPLAB PICkit 2, PICkit 3, PICkit 4, or PICkit 5,
respectively. |
__MPLAB_REALICE__ | When compiling for a Microchip MPLAB REAL ICE™ In-Circuit Emulator. |
__MPLAB_SNAP__ | When compiling for a Microchip MPLAB Snap In-Circuit Debugger. |
__OPTIMIZE_SPEED__ | When using speed-orientated optimizations. |
__OPTIMIZE_SPACE__ and
__OPTIMIZE_SIZE__ | When using space-orientated optimizations. |
__OPTIMIZE_NONE__ | When no optimizations are in effect. |
__OPTIM_FLAGS | Always. Indicates the optimizations in effect (see text following this table). |
__OPTIM_LEVEL | Always. Indicates the optimization level selected, viz.,
0 for -O0 and -Og,
1 for -O1, 2 for
-O2, 3 for -O3, ad
4 for -Os. |
__PICCPRO__ and
__PICC__ | When building for any PIC10/12/14/16 device. |
__PICC18__ | When not in C18 compatibility mode. |
__RESETBITS_ADDR | When the STATUS register will be preserved. Indicates the address at which this register will be saved. |
__SIZEOF_TYPE__ | Always. Indicates the size in bytes of the
specified type, e.g., __SIZEOF_INT__ or
__SIZEOF___INT24__. |
__STACK | Always. Assigned with
__STACK_COMPILED (0x1), __STACK_HYBRID (0x2)
or __STACK_REENTRANT (0x4) to indicate the global stack
setting: compiled, hybrid or software, respectively. |
__STDC_VERSION__ | Always. Assigned a long integer date code in the form
yyyymm to indicate the C Standard
version, e.g., 199901L or 199000L |
__STRICT | When the -Wpedantic option
is enabled. |
__TIME__ | Always. Indicates the current time as a string literal, e.g., “08:06:31” |
__TRADITIONAL18__ | When building for a PIC18 device. Indicates the non-extended instruction set is selected. |
__XC | Always. Indicates MPLAB XC compiler for Microchip is in use. |
__XC8 | Always. Indicates MPLAB XC compiler for Microchip 8-bit devices is in use. |
__XC8_VERSION | Always, and indicates the compiler’s version number (including patch identification) multiplied by 10000, e.g., v4.01.02 would be represented by 40102. |
The compiler-defined macros shown in the following table can be used as
bitwise AND masks to determine the value held by __OPTIM_FLAGS, hence the
optimizations used.
| Macro | Value | Meaning |
|---|---|---|
__OPTIM_NONE | 0x0 | No optimizations applied (on equality). |
__OPTIM_ASM | 0x1 | Assembler optimizations on C code. |
__OPTIM_ASMFILE | 0x2 | Assembler optimizations on assembly source code. |
__OPTIM_1 | 0x100 | Optimization level 1 |
__OPTIM_2 | 0x200 | Optimization level 2 |
__OPTIM_SPEED,
__OPTIM_3 | 0x20000 | Optimized for speed. |
__OPTIM_SPACE,
__OPTIM_SIZE, __OPTIM_S | 0x40000 | Optimized for size. |
__OPTIM_DEBUG,
__OPTIM_G | 0x80000 | Optimized for accurate debug. |
__OPTIM_LOCAL | 0x200000 | Local optimizations applied. |