3.3 Configure LAN8670 Support on SAM E54 Curiosity Ultra Development Board
Note: The SAM E54 Curiosity Ultra Development Board
is presently not supported by Board Support Packages (BSPs) in Zephyr.
However, both the SAM E54 Xplained Pro and the SAM E54 Curiosity Ultra Development Board utilize the same ATSAME54P20A
System-on-Chip (SoC). Therefore, we adapt the device tree source (DTS) file
and pin configuration settings from the SAM E54 Xplained Pro board to align
with the specifications of the SAM E54 Curiosity Ultra Development Board. After these modifications are completed, we
proceed with the compilation of the image file tailored for the SAM E54 Curiosity Ultra Development Board.
- Make sure that the virtual environment is activated.
source ~/zephyrproject/.venv/bin/activate
- Enter the directory.
$ cd zephyrproject/zephyr/
- Open the same54_xpro.dts
file.
$ vim boards/atmel/sam0/same54_xpro/same54_xpro.dts
- In the file make the adaptations as listed below (marked bold in the code section):
/* * Copyright (c) 2019 Benjamin Valentin # Copyright (c) 2024-2025 Gerson Fernando Budke <nandojve@gmail.com> * * SPDX-License-Identifier: Apache-2.0 */ /dts-v1/; #include <atmel/same5xx20.dtsi> #include "same54_xpro-pinctrl.dtsi" #include <zephyr/dt-bindings/input/input-event-codes.h> / { model = "SAM E54 Xplained Pro"; compatible = "same54,xpro", "atmel,same54p20a", "atmel,same54"; chosen {zephyr,console = &sercom1;zephyr,shell-uart = &sercom1;zephyr,sram = &sram0; zephyr,flash = &flash0; }; /* These aliases are provided for compatibility with samples */ aliases { led0 = &led0; pwm-led0 = &pwm_led0; sw0 = &button0; i2c-0 = &sercom7; }; leds { compatible = "gpio-leds"; led0: led_0 { gpios = <&portc 18 GPIO_ACTIVE_LOW>; label = "Yellow LED"; }; }; pwmleds { compatible = "pwm-leds"; pwm_led0: pwm_led_0 { pwms = <&tcc0 2 PWM_MSEC(20)>; }; }; buttons { compatible = "gpio-keys"; button0: button_0 { gpios = <&portb 31 (GPIO_PULL_UP | GPIO_ACTIVE_LOW)>; label = "SW0"; zephyr,code = <INPUT_KEY_0>; }; }; }; &cpu0 { clock-frequency = <120000000>; }; &tcc0 { status = "okay"; compatible = "atmel,sam0-tcc-pwm"; /* Gives a maximum period of 1.1s for 120MHz main clock */ prescaler = <8>; #pwm-cells = <2>; pinctrl-0 = <&pwm_default>; pinctrl-names = "default"; }; &rtc { status = "okay"; counter-mode = "clock"; prescaler = <1024>; atmel,assigned-clocks = <&osc32kctrl 4>; };&sercom1 {status = "okay";compatible = "atmel,sam0-uart";current-speed = <115200>;rxpo = <1>;txpo = <0>;#address-cells = <1>;#size-cells = <0>;pinctrl-0 = <&sercom1_uart_default>;pinctrl-names = "default";};&sercom2 { status = "okay"; compatible = "atmel,sam0-uart"; current-speed = <115200>; rxpo = <1>; txpo = <0>; #address-cells = <1>; #size-cells = <0>; pinctrl-0 = <&sercom2_uart_default>; pinctrl-names = "default"; }; &sercom4 { status = "okay"; compatible = "atmel,sam0-spi"; dipo = <3>; dopo = <0>; #address-cells = <1>; #size-cells = <0>; pinctrl-0 = <&sercom4_spi_default>; pinctrl-names = "default"; }; &sercom7 { status = "okay"; compatible = "atmel,sam0-i2c"; clock-frequency = <I2C_BITRATE_FAST>; #address-cells = <1>; #size-cells = <0>; pinctrl-0 = <&sercom7_i2c_default>; pinctrl-names = "default"; eeprom: eeprom@5e { compatible = "atmel,24mac402"; reg = <0x5e>; }; }; &adc0 { status = "okay"; }; zephyr_udc0: &usb0 { status = "okay"; pinctrl-0 = <&usb_dc_default>; pinctrl-names = "default"; }; &gmac { status = "okay"; pinctrl-0 = <&gmac_rmii>; pinctrl-names = "default";phy-handle = <&phy>;local-mac-address = [04 05 06 01 02 03];max-speed = <10>;}; &mdio { status = "okay";pinctrl-0 = <&mdio_uc_default>;pinctrl-names = "default";phy: ethernet-phy@0 {compatible = "microchip,t1s-phy";reg = <0x0>;plca-enable;plca-node-id = <0>;plca-node-count = <8>;plca-burst-count = <0>;plca-burst-timer = <0x80>;plca-to-timer = <0x20>;status = "okay";};}; &flash0 { partitions { compatible = "fixed-partitions"; #address-cells = <1>; #size-cells = <1>; /* * The final 16 KiB is reserved for the application. * Storage partition will be used by FCB/LittleFS/NVS * if enabled. */ storage_partition: partition@fc000 { label = "storage"; reg = <0x000fc000 0x00004000>; }; }; }; - Open the same54_xpro-pinctrl.dtsi
file.
$ vim boards/atmel/sam0/same54_xpro/same54_xpro-pinctrl.dtsi
- In the file add “mdio_uc_default” and
“sercom1_uart_default” nodes as shown below (marked bold in
the code
section):
/* * Copyright (c) 2022, Gerson Fernando Budke <nandojve@gmail.com> * SPDX-License-Identifier: Apache-2.0 */ #include <dt-bindings/pinctrl/same54p-pinctrl.h> &pinctrl { pwm_default: pwm_default { group1 { pinmux = <PC18F_TCC0_WO2>; }; }; gmac_rmii: gmac_rmii { group1 { pinmux = <PA14L_GMAC_GTXCK>, <PA17L_GMAC_GTXEN>, <PA18L_GMAC_GTX0> <PA19L_GMAC_GTX1>, <PC20L_GMAC_GRXDV>, <PA13L_GMAC_GRX0>, <PA12L_GMAC_GRX1>, <PA15L_GMAC_GRXER>; }; }; mdio_default: mdio_default { group1 { pinmux = <PC11L_GMAC_GMDC>, <PC12L_GMAC_GMDIO>; }; };mdio_uc_default: mdio_uc_default {group1 {pinmux = <PC22L_GMAC_GMDC>,<PC23L_GMAC_GMDIO>;};};sercom7_i2c_default: sercom7_i2c_default { group1 { pinmux = <PD8C_SERCOM7_PAD0>, <PD9C_SERCOM7_PAD1>; }; }; sercom4_spi_default: sercom4_spi_default { group1 { pinmux = <PB26D_SERCOM4_PAD1>, <PB27D_SERCOM4_PAD0>, <PB29D_SERCOM4_PAD3>; }; }; sercom2_uart_default: sercom2_uart_default { group1 { pinmux = <PB25D_SERCOM2_PAD0> <PB24D_SERCOM2_PAD1>; }; };sercom1_uart_default: sercom1_uart_default {group1 {pinmux = <PC27C_SERCOM1_PAD0>,<PC28C_SERCOM1_PAD1>;};};usb_dc_default: usb_dc_default { group1 { pinmux = <PA25H_USB_DP>, <PA24H_USB_DM>; }; }; }; - Save the changes.