This selector allows you to indicate how Device Family Pack (DFP) management should
be performed. The Do not override selection will let the MPLAB
X IDE provide a list of DFPs that can be selected. If you would like to use a DFP
that you have manually downloaded, select User specified
location and then enter the path to the DFP in the Custom
DFP path field. You may also select Compiler
location, which will use the DFPs that ship with the compiler rather
than the IDE.
Custom DFP path
If you have selected User specified location for the
Override default device support option, enter the path to
the DFP you wish to use in this field.
Enables access of const variables directly from flash
Selecting this checkbox enables the const-in-progmem feature, which places
const-qualified objects into program memory space for some
devices. See 3.6.1.5 Const-data-in-progmem Option.
Smart IO default Format
This field allows you to fine-tune the specifications that must be processed by
smart IO functions when the compiler is unable to determine usage information from
the formatted IO function cal. See 3.6.1.14 Smart-io-format Option
Map 32K segments of FLASH into the RAM address space
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.