3.6.6.10 Lto Option

This -flto option runs the standard link-time optimizer.

When invoked with source code, the compiler adds an internal bytecode representation of the code to special sections in the object file. When the object files are linked together, all the function bodies are read from these sections and instantiated as if they had been part of the same translation unit.

To use the link-timer optimizer, specify -flto both at compile time and during the final link. For example:
xc8-cc -c -O3 -flto -mcpu=atmega3290p foo.c
xc8-cc -c -O3 -flto -mcpu=atmega3290p bar.c
xc8-cc -o myprog.elf -flto -O3 -mcpu=atmega3290p foo.o bar.o
Another (simpler) way to enable link-time optimization is:
xc8-cc -o myprog.elf -flto -O3 -mcpu=atmega3290p foo.c bar.c

Link time optimizations do not require the presence of the whole program to operate. If the program does not require any symbols to be exported, it is possible to combine -flto with -fwhole-program to allow the interprocedural optimizers to use more aggressive assumptions which may lead to improved optimization opportunities.

The bytecode files are versioned and there is a strict version check, so bytecode files generated in one version of the XC8 compiler might not work with a different version.

The -fno-lto form of this option does not run the standard link-time optimizer. This is the default action if this option is not specified.