3.7.1.3.3 XC8 Linker - Additional options

Figure 3-8. XC8 Linker - Additional options
Extra linker options
This field allows you to specify additional linker-related options that cannot be otherwise controlled from the IDE. See Wl: Pass Option To The Linker, Option.
Checksum
If required, enter an argument in this field to generate a hash value over data in the HEX file. The argument mimics that used by the -mchecksum option used by MPLAB XC8 for PIC devices, specifically:
start-end@destination[,specifications]
which calculates a hash from start to end addresses, placing the result at destination, and the specifications are as follows:
  • width=n selects the width of the hash result in bytes. A negative width will store the result in little-endian byte order.
  • offset=nnnn specifies an initial value or offset to be added to the hash.
  • algorithm=n selects the hash algorithm to use.
  • code=nn.Base is a hexadecimal code that will trail each byte in the hash result. This can allow each byte of the hash result to be embedded within an instruction.
  • polynomial=nn hexadecimal value which is the polynomial to be used for CRC hashes.
  • revword=n reads the data in reserve order with the word width specified.
  • skip=n.Bytes skips the MSB in the word width specified.
  • xor=n is a hexadecimal value that will be XORed with the hash result before it stored.
Check the MPLAB® XC8 C Compiler User’s Guide for PIC® MCU for full information regarding this option. Note that this field does not map to any compiler option, but will instead trigger a post-build execution of the Hexmate utility.
Trace type
This selector is not yet implemented.
Use response file to link
This field allows a command-line options file to be used by the compiler during the link step, in preference to the other link-step settings in the project properties. See Long Command Lines. This option is only relevant when running MPLAB X IDE under Windows.