4.9.2 Runtime Startup Code
A C program requires certain objects to be initialized and the device to
be in a particular state before it can begin execution of its function
main(). It is the job of the runtime startup code to perform these
tasks, specifically (and in no particular order):
- Initialization of static storage duration objects assigned a value when defined
- Clearing of non-initialized static storage duration objects
- General set up of registers or device state
- Calling the
main()function
One of several runtime startup code object files which provide the runtime startup code is linked into your program.
The runtime startup code assumes that the device has just come out of
Reset and that registers will be holding their power-on-reset value. Note that when the
watchdog or RST_SWRST_bm resets the device, the registers will be reset to
their known, default settings; whereas, jumping to the reset vector will not change the
registers and they will be left in their previous state.
The sections used to hold the runtime startup code are tabulated below.
| Section name | Description |
|---|---|
.init0 | Weakly bound to __init(),
see The Powerup Routine.
If user defines __init(), it will be jumped into immediately
after a reset. |
.init1 | Unused. User definable. |
.init2 | In C programs, weakly bound to code which
initializes the stack and clears __zero_reg__ (r1). |
.init3 | Unused. User definable. |
.init4 | This section contains the code from
libgcc.a that copies the contents of .data
from the program to data memory, as well as the code to clear the
.bss section. |
.init5 | Unused. User definable. |
.init6 | Unused for C programs. |
.init7 | Unused. User definable. |
.init8 | Unused. User definable. |
.init9 | Calls the main()
function. |
The main() function returns to code that is also provided
by the runtime startup code. You can have code executed after main() has
returned by placing code in the sections tabulated below.
| Section name | Description |
|---|---|
.fini9 | Unused. User definable. |
.fini8 | Unused. User definable. |
.fini7 | In C programs, weakly bound to initialize the
stack, and to clear __zero_reg__ (r1). |
.fini6 | Unused for C program. |
.fini5 | Unused. User definable. |
.fini4 | Unused. User definable. |
.fini3 | Unused for C programs. |
.fini2 | Unused. User definable. |
.fini1 | Unused. User definable. |
.fini0 | Goes into an infinite loop after program
termination and completion of any _exit() code (code in the
.fini9 thru .fini1 sections). |