8.9.7 builtin_avr_insert_bits Built-in Function
Inserts bits into val in a manner dictated by a mapping value and
returns the resulting value.
Prototype
uint8_t __builtin_avr_insert_bits (uint32_t map, uint8_t bits, uint8_t val)
Remarks
Insert bits from bits into val in a manner dictated by
map, and return the resulting value.
Each of the 8 nibbles (4 bits) of map controls a bit in the returned
value whose bit position is the same as the nibble's nibble position in
map. For example, the most-significant nibble of
map controls insertion into the most-significant bit of the
returned value, etc. If a nibble in map is 0xF, then the corresponding
bit in the returned value is the corresponding bit of val, unmodified.
Nibbles with a value of 0 through 7 indicate that the corresponding bit in the returned
value is obtained from the bit with bit position within bits.
Example
#include <stdint.h>
#include <stdio.h>
int main(void) {
uint8_t result, myValue, myBits;
volatile char dummy;
myValue = 0xF6;
myBits = 0x3A;
result = __builtin_avr_insert_bits(0x01234567, myBits, myValue);
printf("result is 0x%X\n", result);
result = __builtin_avr_insert_bits(0x5566FFFF, myBits, myValue);
printf("result is 0x%X\n", result);
}
Example Output
result is 0x5C
result is 0xC6
Example Explanation
In the first usage of the built-in in the above example, the first nibble in the
map value (0x0) indicates that the most-significant bit of the
result will be derived from bit #0 in myBits. The next
lower-significant bit will be derived from bit #1, etc. Given the map nibbles in the
above example, the first execution of the built-in will return a value being that of
myBits with its bits appearing in reverse order.
In the second usage of the built-in, the lower four nibble of map are
0xF, which implies that the lower four bits of the result value will be the lower four
bits of myValue, unmodified. The two most-significant nibbles of
map are 0x5, indicating that the two most-significant bits of the
returned value will be bit #5 of myBits (which is 1). Similarly, the
next two bits of the result will be bit #6 of myBits (which is 0).