4.14.2 Changing and Linking the Allocated Section
The location of the default sections in which functions and objects are placed can be changed via driver options. The default sections the compiler uses to hold objects and code are listed in Compiler-Generated Sections.
The __section() specifier allows you to have a object or
function redirected into a user-define section. This allows you to relocate individual
objects or functions.
Objects that use the __section() specifier will be
cleared or initialized in the usual way by the runtime startup code.
__section() specifier, the CCI (see Ext Option) must be
enabled.int __section("myBss") foobar;
int __section("myText") helper(int mode) { /* ... */ }-Wl,--section-start=section=addr
option when building (linking) your program, provided that the linker script has already
defined an output section with the same name. If this is not the case, then you might need
to copy the default linker script, modify it appropriately, and specify it using the
-Tscript driver option. The modification must
define an output section using the same name as the section you have specified. The
following, for example, will allocate any input sections called myBss to
the output section with the same name.myBss :
{
KEEP(*(myBss))
}Note that you need to use an offset of 0x800000 for any address that is in the data space.
For example, suppose you wish to place the new myBss section, created
above, at SRAM address 0x300, use an option similar to:
-Wl,--section-start=myBss=0x800300
The -Wl,-Tsection=addr option can be
used to position standard sections, like the .text, .data
and .bss sections; however, since a Best Fit Allocator (BFA) is used with
MPLAB XC8, these sections are not commonly used by the compiler to store objects or
code.
Although the -Wl,-Ttext=addr option will move the
.text section to the offset specified, this option also sets the
starting address from which the linker begins program memory allocation for all code (even
that handled by the BFA). Thus, when this option is used, the .text
section will start at the exact offset specified; other code sections will be located after
this. Similarly, the -Wl,-Tdata=addr option also sets the
starting address from which the linker begins data (both initialized and uninitialized)
allocation.