4.7.2 Function Attributes
The compiler keyword __attribute__() allows you to specify special
attributes of functions. Place inside the parentheses following this keyword a
comma-separated list of the relevant attributes, for example:
__attribute__((weak))
The attribute can be placed anywhere in the object’s definition, but is usually placed as in the following example.
char __attribute__((weak)) input(int mode);
char input(int mode) __attribute__((weak));