4.8.2 Changing the Default Interrupt Function Allocation
You can use the __at() specifier (see Changing the Default Function Allocation) if you want to move
the interrupt function itself. This does not alter the position of the vector table, but
the appropriate table entry will still point to the correct address of the shifted
function.