4.13.1.1 Preprocessor Arithmetic
Preprocessor macro replacement expressions are textual and do not utilize types. Unless they are part of the controlling expression to the inclusion directives (discussed below), macros are not evaluated by the preprocessor. Once macros have been textually expanded and preprocessing is complete, the expansion forms a C expression which is evaluated by the code generator along with other C code. Tokens within the expanded C expression inherit a type, with values then subject to integral promotion and type conversion in the usual way.
If a macro is part of the controlling expression to a conditional
inclusion directive (#if or #elif), the macro must be
evaluated by the preprocessor. The result of this evaluation is sometimes different from
the C-domain result for the same sequence. The preprocessor processes unsigned and signed
literal integer values in the controlling expression as if they had the respective type
uintmax_t or intmax_t, defined in
<stdint.h>. For the MPLAB XC8 C Compiler, the size of these types is 64 bits.