7.8 I/O Memory
All ATtiny1614/1616/1617 Automotive I/Os and peripherals are
located in the I/O memory space. The I/O address range from 0x00 to 0x3F can be accessed
in a single cycle using IN and OUT instructions. The
extended I/O memory space from 0x0040 - 0x0FFF can be accessed by the
LD/LDS/LDD and
ST/STS/STD instructions,
transferring data between the 32 general purpose working registers and the I/O memory
space.
I/O registers within the address range 0x00 - 0x1F are directly bit
accessible using the SBI and CBI instructions. In
these registers, the value of single bits can be checked by using the
SBIS and SBIC instructions. Refer to the
Instruction Set section for more details.
For compatibility with future devices, reserved bits should be written to zero if accessed. Reserved I/O memory addresses should never be written.
Some of the interrupt flags are cleared by writing a '1' to them. On ATtiny1614/1616/1617 Automotive devices, the CBI and
SBI instructions will only operate on the specified bit and can be
used on registers containing such interrupt flags. The CBI and
SBI instructions work with registers 0x00 - 0x1F only.
General Purpose I/O Registers
The ATtiny1614/1616/1617 Automotive devices provide four general
purpose I/O registers. These registers can be used for storing any information, and they
are particularly useful for storing global variables and interrupt flags. general
purpose I/O registers, which reside in the address range 0x1C - 0x1F, are directly bit
accessible using the SBI, CBI, SBIS,
and SBIC instructions.