3.5.1 What’s the Difference Between the Free and PRO Modes?
These modes, or editions, mainly differ in the optimizations that are performed when compiling (see 21 Optimizations). Compilers operating in Free mode can compile for all the same devices as supported by the Pro mode. The code compiled in Free or PRO modes can use all the available memory for the selected device. What will be different is the size and speed of the generated compiler output. Free mode output will be less efficient when compared to that produced in Pro mode.