8.8 Constant Types and Formats

A constant is used to represent a numerical value in the source code, for example 123 is a constant. Like any value, a constant must have a C/C++ type. In addition to a constant’s type, the actual value can be specified in one of several formats. The format of integral constants specifies their radix. MPLAB XC32 C/C++ supports the ANSI standard radix specifiers as well as ones which enables binary constants to be specified in C code.

The formats used to specify the radices are given in Table 8-4. The letters used to specify binary or hexadecimal radices are case insensitive, as are the letters used to specify the hexadecimal digits.

Table 8-3. RADIX FORMATS
Radix Format Example
binary 0b number or 0B number 0b10011010
octal 0 number 0763
decimal number 129
hexadecimal 0x number or 0X number 0x2F

Any integral constant will have a type of int, long int or long long int, so that the type can hold the value without overflow. Constants specified in octal or hexadecimal may also be assigned a type of unsigned int, unsigned long int or unsigned long long int if the signed counterparts are too small to hold the value.

The default types of constants may be changed by the addition of a suffix after the digits, e.g., 23U, where U is the suffix. Table 8-5 shows the possible combination of suffixes and the types that are considered when assigning a type. So, for example, if the suffix l is specified and the value is a decimal constant, the compiler will assign the type long int, if that type will hold the constant; otherwise, it will assigned long long int. If the constant was specified as an octal or hexadecimal constant, then unsigned types are also considered.

Table 8-4. SUFFIXES AND ASSIGNED TYPES
SuffixDecimalOctal or Hexadecimal
u or Uunsigned int

unsigned long int

unsigned long long int

unsigned int

unsigned long int

unsigned long long int

l or Llong int

long long int

long int

unsigned long int

long long int

unsigned long long int

u or U, and l or Lunsigned long int

unsigned long long int

unsigned long int

unsigned long long int

ll or LLlong long intlong long int

unsigned long long int

u or U, and ll or LLunsigned long long intunsigned long long int

Here is an example of code that may fail because the default type assigned to a constant is not appropriate:

unsigned long int result;
unsigned char shifter;

int main(void)
{
    shifter = 40;
    result = 1 << shifter;
    // code that uses result
}

The constant 1 will be assigned an int type hence the result of the shift operation will be an int and the upper bits of the long variable, result, can never be set, regardless of how much the constant is shifted. In this case, the value 1 shifted left 40 bits will yield the result 0, not 0x10000000000.

The following uses a suffix to change the type of the constant, hence ensure the shift result has an unsigned long type.

result = 1UL << shifter;

Floating-point constants have double type unless suffixed by f or F, in which case it is a float constant. The suffixes l or L specify a long double type.

Character constants are enclosed by single quote characters, , for example ’a’. A character constant has int type, although this may be optimized to a char type later in the compilation.

Multi-byte character constants are accepted by the compiler but are not supported by the standard libraries.

String constants, or string literals, are enclosed by double quote characters “ ”, for example “hello world”. The type of string constants is const char * and the character that make up the string are stored in the program memory, as are all objects qualified const.

To comply with the ANSI C standard, the compiler does not support the extended character set in characters or character arrays. Instead, they need to be escaped using the backslash character, as in the following example:

const char name[] = “Bj\370rk”;

printf(“%s's Resum\351”, name); \\ prints “Bjørk's Resumé”

Assigning a string literal to a pointer to a non-const char will generate a warning from the compiler. This code is legal, but the behavior if the pointer attempts to write to the string will fail. For example:

char * cp= “one”; // “one” in ROM, produces warning

const char * ccp= “two”; // “two” in ROM, correct

Defining and initializing a non-const array (i.e., not a pointer definition) with a string,

char ca[]= “two”; // “two” different to the above

is a special case and produces an array in data space which is initialized at start-up with the string “two” (copied from program space), whereas a string constant used in other contexts represents an unnamed const-qualified array, accessed directly in program space.

The MPLAB XC32 C/C++ Compiler will use the same storage location and label for strings that have identical character sequences. For example, in the code snippet

if(strncmp(scp, “hello world”, 6) == 0)
   fred = 0;
if(strcmp(scp, “hello world”) == 0)
   fred++;

the two identical character string greetings will share the same memory locations. The link-time optimization must be enabled to allow this optimization when the strings may be located in different modules.

Two adjacent string constants (i.e., two strings separated only by white space) are concatenated by the compiler. Thus:

const char * cp = “hello” “ world”;

will assign the pointer with the address of the string “hello world”.