5.2 XC32 Assembler Options

The following are assembler feature controls displayed in the MPLAB X IDE and VS Code project property dialogs, along with their corresponding driver options. When used, these options are passed to the assembler application xc32-as and are not relevant for the xc32-gcc driver. For additional assembler options, see MPLAB® XC32 Assembler, Linker And Utilities User’s Guide documentation.

Table 5-2. XC32 Assembler General Category
OptionDescriptionCommand Line
Have symbols in production buildGenerate debugging information for source-level debugging in MPLAB X.--gdwarf-2
Keep local symbolsCheck to keep local symbols, i.e., labels beginning with .L (upper case only).

Uncheck to discard local symbols.

--keep-locals

See MPLAB® XC32 Assembler, Linker and Utilities User's Guide.

Preprocessor macro definitionsProject-specific preprocessor macro defines passed via the compiler's –D option.

-Dmacro[=defn] See MPLAB® XC32 Assembler, Linker and Utilities User's Guide.

Assembler symbolsDefine symbol 'sym' to a given 'value'.--defsym sym=value

See MPLAB® XC32 Assembler, Linker and Utilities User's Guide.

Preprocessor Include directoriesRelative paths are from MPLAB X project directory.

-I dir See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Assembler Include directoriesRelative paths are from MPLAB X project directory.

Add a directory to the list of directories the assembler searches for files specified in .include directives.

You may add as many directories as necessary to include a variety of paths. The current working directory is always searched first and then -I directories in the order in which they were specified (left to right) here.

-I dir

See MPLAB® XC32 Assembler, Linker and Utilities User's Guide.

Table 5-3. XC32 Assembler Other Options Category
OptionDescriptionCommand Line
Diagnostics levelSelect warnings to display in the Output window. Select “Generate warnings” to have the usual warnings issued by the compiler; “Suppress warnings”to have only errors displayed, and "Fatal Warnings" to have the assembler treat warnings as if they were errors.--[no-]warn

--fatal-warnings See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Include source codeCheck for a high-level language listing. High-level listings require that the assembly source code is generated by a compiler, a debugging option like -g is given to the compiler, and assembly listings (-al) are requested.

Uncheck for a regular listing.

-ah

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Expand macrosCheck to expand macros in a listing.

Uncheck to collapse macros.

-am

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Include false conditionalsCheck to include false conditionals (.if, .ifdef) in a listing.

Uncheck to omit false conditionals.

-ac

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Omit forms processingCheck to turn off all forms processing that would be performed by the listing directives .psize, .eject, .title and .sbttl.

Uncheck to process by listing directives.

-an

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Include assemblyCheck for an assembly listing. This -a suboption may be used with other suboptions.

Uncheck to exclude an assembly listing.

-al

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

List symbolsCheck for a symbol table listing.

Uncheck to exclude the symbol table from the listing.

-as

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

Omit debugging directivesCheck to omit debugging directives from a listing. This can make the listing cleaner.

Uncheck to included debugging directives.

-ad

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide

List to fileUse this option if you want the assembly listing for any assembly source files in the project.

They will have the same basename as the source, with a .lst extension.

-a=file.lst

See the MPLAB® XC32 Assembler, Linker and Utilities User's Guide