10.4 Variables in Program Memory

The only variables that are placed into program memory are those that are not auto and which have been qualified const. Any auto variables qualified const are placed on the stack along with other auto variables.

Any const-qualified (auto or non-auto) variable will always be read-only and any attempt to write to these in your source code will result in an error being issued by the compiler.

A const object is usually defined with initial values, as the program cannot write to these objects at runtime. However, this is not a requirement. An uninitialized const object is allocated space in the bss section, along with other uninitialized RAM variables, but is still treated as read-only by the compiler.

const char IOtype = 'A'; // initialized const object

const char buffer[10]; // I just reserve memory in RAM