23.3.2 Pragmas to Control Options/Optimization

#pragma GCC target ("string" ...)

This pragma may be used to set target-specific options for all subsequent function definitions. The arguments allowed are any options prefixed with -m, such that -m will be prepended to each string given to form the target options, i.e., #pragma GCC target ("arch=armv7e-m"). All function definitions following this pragma will behave as if the attribute ((target("string")) were applied to the definition. The parentheses are optional.

#pragma GCC optimize ("string" ...)

The #pragma GCC optimize ("string"...) pragma sets default optimization attributes for function declarations and definitions that do not otherwise specify these attributes. All functions after the pragma will be optimized accordingly. The parentheses are optional. The arguments allowed may be:
  • A number n, to be interpreted as an optimization level, i.e., the -On option
  • A string beginning with O, which is interpreted as an optimization option, i.e., -Ostring
  • Otherwise, string should be an option that can be used with a -f prefix.
The #pragma GCC reset_options pragma clears the default optimizations, so that the optimization of subsequent functions is not controlled by optimize pragma.

#pragma GCC push_options

#pragma GCC pop_options

These pragmas allow for maintaining a stack of target and optimize options. The push_options pragma will push the current options onto the stack, which will be the command-line options if no target or optimize pragma are in effect. The pop_options will restore the options in effect to those last pushed onto the stack.

#pragma GCC reset_options

Clears any current options set via the target or optimize pragmas for all subsequent function definitions.