8.5.1 CMCC-based Tightly-Coupled Memory

Some SAM microcontrollers based on the Cortex®-M4, such as the SAME54 or SAMD51, feature a ARM Cortex-M Cache Controller (CMCC) peripheral. With CMCC, a part of the cache can be used as Tightly-Coupled Memory (TCM) for deterministic code performance by loading the critical code in a WAY and locking it.

To have functions and objects placed into CMCC-based TCM, use the tcm attribute with those functions and objects which need to be repositioned, then use the -mtcm=size option to set the size (in bytes) of the TCM and ensure that the device-specific runtime startup code and linker script configure the TCM. The size specified must be one permitted by the device and can be specified as a decimal number or as a hexadecimal number with a leading 0x. When an invalid size has been specified, check the error message to see the sizes acceptable by that device. Once enabled, the preprocessor macro __XC32_TCM_LENGTH will be defined and equated to the size of the TCM area.