3.1 Other TMR1 Features
The following table shows how some of the other features of TMR1 can be applied using UTMR:
| Feature | TMR1 | UTMR |
|---|---|---|
| Active Clock Edge | TMR1 increments at every rising edge of clock. In some cases, a falling edge must be registered before the timer starts incrementing. | Set CPOL = Rising Clock Edge to increment UTMR at rising clock edges. |
| Synchronization | TMR1 can operate either synchronous or asynchronous to the system clock based on SYNC bit setting. | UTMR always operates asynchronous to the system clock. The CSYNC bit is used to synchronize signals and commands going in and out of the UTMR module. |
| Buffered Read/Write | RD16 bit can be used to read/write 16-bits of TMRxH:L register in one atomic operation. | The TUxyTMR timer/counter register is not guarded for atomic access. However, the TUxyPR period register is double-buffered. Refer to section 1.1 UTMR Size and Buffered Access for details on UTMR buffered access to registers. |
| Prescaler | TMR1 has 4 programmable input prescaler options ranging from 1:1 to 1:8, which can be selected using CKPS bits. | UTMR has 256 programmable clock prescaler options ranging from 1:1 to 1:256, which can be selected using TUxyPS register. |
| Gate Source and Polarity | The gate source is selected using GSS bits and the polarity of the gate source is selected using GPOL bit. | The ERS signal acts as the gate source and can be selected using TUxyERS register. The ERS polarity can be selected using EPOL bit. |
| Gate Value Status | The most current value of gate level can be read using GVAL bit. | Use OM = Level output to represent the current run/stop state of UTMR, i.e. when the gate is activated and when it is not active. This is also represented using the RUN status bit. |
| Output | TMR1 output pulses every roll-over for one instruction clock. | Set TUxyPR to the maximum value and set OM = Pulse Output mode. This will cause a pulse for one timer clock period when the timer rolls over. |
| Interrupts | The TMRxGIF gate event interrupt occurs at the completion of a gate event. The TMRxIF timer interrupt occurs when the counter rolls-over to zero. | CIF capture interrupt can be used to signify completion of a gate event. ZIF zero interrupt can be used to signify a counter roll-over. |
| Sleep Mode Operation | TMR1 halts when operating synchronously. In asynchronous mode, TMR1 continues operating as long as the clock is active, and wakes up the CPU if interrupts are enabled. | UTMR continues to operate as long as the clock is active, and wakes up the CPU if interrupts are enabled. |