In some scenarios, using a system impedance instead of matching directly to the target value is
preferred. An example is the connection of a SAW filter to an LNA. The SAW filter has a
certain complex impedance, which are available in the technical documents. The SAW
manufacturer typically recommends a matching network to 50Ω impedance. Typically, this
does not fit the input of the LNA, and it must be matched to the 50Ω impedance. This
point is called the system impedance. From the technical point of view, this
transformation is not needed, as it is possible to directly transform from the complex
impedance of the LNA to the value of the SAW. This can be a difficult task with complex
equations. Therefore, using the system impedance is helpful. The big advantage is the
defined point that can be used to perform the matching for both RF components, as shown
in the following figure.Figure 3-3. Application Example System
Impedance
The online versions of the documents are provided as a courtesy. Verify all content and data in the device’s PDF documentation found on the device product page.