21.2 Preprocessing Directives
The compiler accepts several specialized preprocessor directives in addition to the standard directives. All of these are listed in the following table.
| Directive | Meaning | Example |
|---|---|---|
#define | Define preprocessor macro | #define SIZE 5
|
#elif | Short for #else #if | see #ifdef |
#else | Conditionally include source lines | see #if |
#endif | Terminate conditional source inclusion | see #if |
#error | Generate an error message | #error Size too big |
#if | Include source lines if constant expression true | #if SIZE < 10
|
#ifdef | Include source lines if preprocessor symbol defined | #ifdef FLAG
|
#ifndef | Include source lines if preprocessor symbol not defined | #ifndef FLAG
|
#include | Include text file into source | #include <stdio.h>
|
#line | Specify line number and file name for listing | #line 3 final |
#pragma | Compiler-specific options | #pragma config
WDT=OFF |
#undef | Undefines preprocessor symbol | #undef FLAG |
#warning | Generate a warning message | #warning Length not
set |
Macro expansion using arguments can use the # character
to convert an argument to a string, and the ## sequence to concatenate
arguments. If two expressions are being concatenated, consider using two macros in case
either expression requires substitution itself, so for example
#define paste1(a,b) a##b
#define paste(a,b) paste1(a,b)
lets you use the paste macro to concatenate two
expressions that themselves may require further expansion. Remember that once a macro
identifier has been expanded, it will not be expanded again if it appears after
concatenation.
For implementation-defined behavior of preprocessing directives, see thePreprocessing Directivessection.