5.5.3 How Can I Make My Code Smaller?
General advice for creating smaller code:
- Do not mix data types.
- Define index variables in the native word width.
- Don't use floating-point variables when integers will suffice. When using floating-point variables, consider using the smaller math libraries.
- Compiler option
-mpacan be combined with any optimization level to reduce code size. See the following chapter in this user’s guide:Note: Optimized code may be more difficult to debug. - When initializing an SFR, use the full name of the SFR instead of bit names. You can initialize several fields at once with this technique.
- Instead of copying code literally into several places in your program, reorganize the shared code into functions.
- Use the small code, small scalar, and large data memory models. Refer to the following section of this user’s guide: