16.2 Runtime Startup and Initialization
A C program requires certain objects to be initialized and the processor
to be in a particular state before it can begin execution of its function
main(). It is the job of the runtime startup code to perform these
tasks, specifically (and in no particular order):
- Initialization of global variables assigned a value when defined
- Initialization of the stack
- Clearing of non-initialized global variables
- General setup of registers or processor state
Two C run-time startup modules are included in the
libc99-pic30-elf.a archive/library. The entry point for both startup
modules is __reset. The linker scripts construct a GOTO
__reset instruction at location 0 in program memory, which transfers control
upon device Reset.
The primary startup module is linked by default and performs the following:
- The Stack Pointer (W15) and Stack Pointer Limit register (SPLIM) are initialized, using values provided by the linker or a custom linker script (see the 7.3 Stack section for more information).
- If a
.constsection is defined, it is mapped into the Program Space Visibility (PSV) window by initializing the PSV page and CORCON registers, as appropriate, ifconst-in-codememory mode is used or variables have been explicitly allocated tospace(auto_psv). - The data initialization template is read, causing all uninitialized objects to be cleared and all initialized objects to be initialized with values read from program memory. The data initialization template is created by the linker.Note: Persistent data is never cleared or initialized.
- If the application has defined
user_initfunctions (see section 14.1.2 Function Attributes), these are invoked. The order of execution depends on link order. - The function
main()is called with no parameters. - If
main()returns, the processor will reset.
The alternate startup module is linked when the -Wl,
--no-data-init option is specified. It performs the same operations,
except for step (3), which is omitted. The alternate startup module is smaller than the
primary module, and can be selected to conserve program memory if data initialization is
not required.
Zipped source code (in dsPIC DSC assembly language) for both modules is
provided in the <xc-dsc install
directory>\src\libpic30.zip. The startup modules may be modified if
necessary. For example, if an application requires main to be called with
parameters, a conditional assembly directive may be changed to provide this support.
You can override the normal startup behavior by defining the function
int _crt_start_mode(void). This function should return 0 to indicate
that a normal start up procedure is used. Any other return value will indicate that
preserved variables should not be initialized. If you have not defined
this function, the compiler will always initialize everything.