2.4.4.1 Response Code operation
The Response Code operation is used by server to notify the result of operation issued from client.
The OTACP Response Code is variable length and the format is defined in Table 4.1.
| Opcode | Requirement | Size (octets) | Description |
|---|---|---|---|
| 0x01 | M | 1 | Response Code |
| Opcode | Requirement | Size (octets) | Description |
| Request_Opcode | M | 1 | Request Opcode |
| Result_Code | M | 1 | Result Code |
| Response_Parameter | O | Variables | Dependent of the Request Opcode |
The Result Codes are defined in Table 4.2:
| Result Code | Definition | Description |
|---|---|---|
| 0x00 | Success | Response for successful operation. |
| 0x01 | Invalid State | Response if the requested operation is not valid in the current state of the firmware update process. |
| 0x02 | Not Supported | Response if unsupported Opcode is received. |
| 0x03 | Operation Failed | Response if the requested operation failed. |
| 0x04 | Invalid Parameter | Response if Parameter received does not meet the requirements of the service. |
| 0x05 | Unspecified Error | The server has encountered an unspecified error. |
| 0x06 | Reserved for future use | - |