BLE_OTAPS_SetEncrytionInfo
C
uint16_t BLE_OTAPS_SetEncrytionInfo(uint8_t * p_iv, uint8_t * p_key);
Description
Set IV value and encryption key of AES-CBC for OTA DFU new image decryption.
Application must call this API before starting BLE OTA procedure if image is encrpyted.
Parameters
Parameter | Description |
---|---|
[in] p_iv | Pointer to the 16 bytes IV value. |
[in] p_key | Pointer to the 16 bytes encryption key. |
Return values
Return value | Description |
---|---|
MBA_RES_SUCCESS | Successfully set IV value and Key. |
MBA_RES_BAD_STATE | Failure because the BLE OTA is in progress. |