GATTS_EncDataKeyMatlRsp
PIC32CX-BZ6
C
uint16_t GATTS_EncDataKeyMatlRsp(uint16_t connHandle, uint8_t *p_key, uint8_t *p_iv);
Description
Responds to a GATT client's request for encrypted data key material.
Note
This function should be called upon receiving the GATTS_EVT_ENC_DATA_KEY_MATL_REQ event.If either p_key or p_iv is NULL, the read request will be rejected.
Parameters
Parameter | Description |
---|---|
[in] connHandle | Connection handle for sending the response. |
[in] p_key | Pointer to the 16-byte shared session key. |
[in] p_iv | Pointer to the 8-byte initialization vector. |
Return values
Return value | Description |
---|---|
MBA_RES_SUCCESS | Response successfully initiated. |
MBA_RES_FAIL | Operation not permitted; no corresponding read request received. |
MBA_RES_OOM | Memory allocation failure occurred internally. |
MBA_RES_INVALID_PARA | Invalid parameters, such as an invalid connection handle. |