GATTS_SendHandleValue

C

uint16_t GATTS_SendHandleValue(uint16_t connHandle, GATTS_HandleValueParams_T *p_hvParams);

Description

Sends a Handle Value Notification or Indication to a GATT client.

Note

The type of message sent (notification or indication) is determined by the sendType field in the [GATTS_HandleValueParams_T](GUID-D758F481-1634-4570-8B84-F76195710D2F.md) structure. sendType in [GATTS_HandleValueParams_T](GUID-D758F481-1634-4570-8B84-F76195710D2F.md) determines if a notification or Indication is sent. A notification or indication can be sent only if the property matches and the CCCD value is configured to be enabled.

Events generated

GATTS_EVT_HV_CONFIRM is generated if an indication is successfully sent. ATT_EVT_TIMEOUT is generated if the client does not respond to an indication.

Parameters

ParameterDescription
[in] connHandleHandle of the connection to send Handle Value Notification/Indication.
[in] p_hvParamsPointer to the parameters for the Handle Value operation. See GATTS_HandleValueParams_T.

Return values

Return valueDescription
MBA_RES_SUCCESSOperation successfully started.
MBA_RES_FAILOperation failed due to invalid permissions or unavailable memory.
MBA_RES_OOMMemory allocation failure occurred internally.
MBA_RES_INVALID_PARAInvalid parameters, such as an invalid connection handle or out-of-range values.
MBA_RES_BUSYAn indication is already in progress.
MBA_RES_NO_RESOURCENo resources available to send the handle value.