BLE_OTAPC_FeatureDisc
C
uint16_t BLE_OTAPC_FeatureDisc(uint16_t connHandle);
Description
Initiates a feature discovery operation.
Note
An event of type BLE_OTAPC_EVT_FEATURE_IND will be generated upon completion of the procedure.
Parameters
Parameter | Description |
---|---|
[in] connHandle | The connection handle for which to perform feature discovery. |
Return values
Return value | Description |
---|---|
MBA_RES_BAD_STATE | The OTA profile is not in the correct state to perform this operation. |